<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Cannot flash program RT1064, Internal Flash Driver Reports Error. in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Cannot-flash-program-RT1064-Internal-Flash-Driver-Reports-Error/m-p/932179#M2205</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When attempting to load code onto my RT 1064 EVK,&amp;nbsp;the flash driver reports the following error:&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ProgramPage (0x70000000, 0x200026C8, 0x4000) status 0x1 - driver reported driver error - EXTSPIJ driver rc 185 (0xB9)&lt;BR /&gt;Closing flash driver MIMXRT1064.cfx&lt;BR /&gt;Target error from Commit Flash write: Ef(49): Flash driver operation gave error.&lt;BR /&gt;GDB stub (crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I am using MCUXpresso 11.0 and have successfully preformed a mass erase of the flash and reset the board, but this has not helped the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also able to connect to the board and erase the flash with the SW7 switch in position 0010 (internal flash selected as boot device), which leads me to believe that a bad image is not the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This&amp;nbsp;all started after I used the GUI flash tool to put a .bin file of the iled example code into flash (location 0x70000000), but it now seems that I can't load anything on the board or recover it via the normal methods.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated. Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 31 Aug 2019 21:40:41 GMT</pubDate>
    <dc:creator>thimsenma</dc:creator>
    <dc:date>2019-08-31T21:40:41Z</dc:date>
    <item>
      <title>Cannot flash program RT1064, Internal Flash Driver Reports Error.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Cannot-flash-program-RT1064-Internal-Flash-Driver-Reports-Error/m-p/932179#M2205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When attempting to load code onto my RT 1064 EVK,&amp;nbsp;the flash driver reports the following error:&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ProgramPage (0x70000000, 0x200026C8, 0x4000) status 0x1 - driver reported driver error - EXTSPIJ driver rc 185 (0xB9)&lt;BR /&gt;Closing flash driver MIMXRT1064.cfx&lt;BR /&gt;Target error from Commit Flash write: Ef(49): Flash driver operation gave error.&lt;BR /&gt;GDB stub (crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I am using MCUXpresso 11.0 and have successfully preformed a mass erase of the flash and reset the board, but this has not helped the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also able to connect to the board and erase the flash with the SW7 switch in position 0010 (internal flash selected as boot device), which leads me to believe that a bad image is not the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This&amp;nbsp;all started after I used the GUI flash tool to put a .bin file of the iled example code into flash (location 0x70000000), but it now seems that I can't load anything on the board or recover it via the normal methods.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated. Thanks!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Aug 2019 21:40:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Cannot-flash-program-RT1064-Internal-Flash-Driver-Reports-Error/m-p/932179#M2205</guid>
      <dc:creator>thimsenma</dc:creator>
      <dc:date>2019-08-31T21:40:41Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot flash program RT1064, Internal Flash Driver Reports Error.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Cannot-flash-program-RT1064-Internal-Flash-Driver-Reports-Error/m-p/932180#M2206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and&lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;I'd like to confirm that the MIMXRT1064 would be non-programmable after programming one of your programs, even example demos is disabled to be programmed again, is it right?&lt;BR /&gt;Meanwhile, I'd like you can try these below methods to fix this issue.&lt;BR /&gt;1. Update the firmware of the on-board debugger OpenSDA.&lt;BR /&gt;2. Adapt the SW7 to select Serial Downloader mode, then try to program the i.MX RT1064 under this mode, then recover to the Interteral Boot to boot.&lt;BR /&gt;BTW, you can download the NXP-MCUBootUtility via the link&lt;BR /&gt;&lt;A class="" data-content-finding="Community" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fgithub.com%2FJayHeng%2FNXP-MCUBootUtility%2Freleases%2Ftag%2Fv1.4.0" rel="nofollow" target="_blank"&gt;https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v1.4.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 02:05:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Cannot-flash-program-RT1064-Internal-Flash-Driver-Reports-Error/m-p/932180#M2206</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-09-03T02:05:35Z</dc:date>
    </item>
  </channel>
</rss>