<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックProgramming release code to MK02FN64 via MCUXPresso</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Programming-release-code-to-MK02FN64-via-MCUXPresso/m-p/712644#M219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to program and run release code to my target using&amp;nbsp;MCUXpresso, without any debug mode overhead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My programming interface is a PEMicro Multilink Universal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have created a "run" configuration that references the release build of my code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I click "run", MCUXPresso starts a debug session, and never asks me about what hardware interface I'd like to use (or even what port the target is on).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The debug session doesn't have an interface for termination (right clicking simply gives an option to "re-launch")&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am lost as to how to run my code without starting a debug session.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Aug 2017 19:07:36 GMT</pubDate>
    <dc:creator>arjuniyer</dc:creator>
    <dc:date>2017-08-31T19:07:36Z</dc:date>
    <item>
      <title>Programming release code to MK02FN64 via MCUXPresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Programming-release-code-to-MK02FN64-via-MCUXPresso/m-p/712644#M219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to program and run release code to my target using&amp;nbsp;MCUXpresso, without any debug mode overhead.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My programming interface is a PEMicro Multilink Universal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have created a "run" configuration that references the release build of my code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I click "run", MCUXPresso starts a debug session, and never asks me about what hardware interface I'd like to use (or even what port the target is on).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The debug session doesn't have an interface for termination (right clicking simply gives an option to "re-launch")&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am lost as to how to run my code without starting a debug session.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 19:07:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Programming-release-code-to-MK02FN64-via-MCUXPresso/m-p/712644#M219</guid>
      <dc:creator>arjuniyer</dc:creator>
      <dc:date>2017-08-31T19:07:36Z</dc:date>
    </item>
    <item>
      <title>Re: Programming release code to MK02FN64 via MCUXPresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Programming-release-code-to-MK02FN64-via-MCUXPresso/m-p/712645#M220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I experienced the similar problem as yours when I use MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;if the connection and firmware has no problem, most of times, I can fix the problem by removing all .launch files in the project.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/27935i4B905CEC610250D7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if removing .launch file can not solve the problem, try create a NEW project in a NEW workspace and see how the connection works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Sep 2017 04:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Programming-release-code-to-MK02FN64-via-MCUXPresso/m-p/712645#M220</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2017-09-05T04:24:53Z</dc:date>
    </item>
  </channel>
</rss>