<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: Running KDS 3.2 alongside MCUXpresso on Linux</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615441#M21</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leroy,&lt;/P&gt;&lt;P&gt;sorry, yes you are right, removing the file won't do the trick. Your procedure will :smileywink: Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Zdar&lt;/P&gt;&lt;P&gt;MCUXpresso support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Mar 2017 12:03:39 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2017-03-28T12:03:39Z</dc:date>
    <item>
      <title>Running KDS 3.2 alongside MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615436#M16</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I noticed that the installation of MCUXpresso fails because of a conflict with KDS 3.2.0.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;dpkg: error processing archive mcuxpressoide-10.0.0_344.x86_64.deb (--install):&lt;/P&gt;&lt;P&gt;&amp;nbsp;trying to overwrite '/lib/udev/rules.d/55-pemicro.rules', which is also in package kinetis-design-studio 3.2.0&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;It's pretty clear what's going wrong, but I don't know if I can fix this without repackaging either application. Can this be looked at for the next release?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 19:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615436#M16</guid>
      <dc:creator>gmb</dc:creator>
      <dc:date>2017-03-23T19:55:58Z</dc:date>
    </item>
    <item>
      <title>Re: Running KDS 3.2 alongside MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615437#M17</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Greg,&lt;/P&gt;&lt;P&gt;yes, this is a problem we will definitely investigate. Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Mar 2017 08:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615437#M17</guid>
      <dc:creator>michalzan</dc:creator>
      <dc:date>2017-03-24T08:35:40Z</dc:date>
    </item>
    <item>
      <title>Re: Running KDS 3.2 alongside MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615438#M18</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a workaround for this issue? I'm just "playing" at the moment so not a large deal if not. I assume uninstalling KDS would do the trick but I'm not at the point where I want to do this yet. Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leroy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Mar 2017 13:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615438#M18</guid>
      <dc:creator>leroyle</dc:creator>
      <dc:date>2017-03-27T13:43:45Z</dc:date>
    </item>
    <item>
      <title>Re: Running KDS 3.2 alongside MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615439#M19</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;P&amp;amp;E udev rules for KDS are exactly the same as the ones for MCUXpresso, so as a workaround you can just delete the file (/lib/udev/rules.d/55-pemicro.rules) and it will get back there with installation of the&amp;nbsp;MCUXpresso and you will be able to use both IDEs. Let us know if you have any other questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;zdar,&lt;/P&gt;&lt;P&gt;MCUXpresso support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Mar 2017 18:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615439#M19</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-03-27T18:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: Running KDS 3.2 alongside MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615440#M20</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks zdar for that response back.&lt;/P&gt;&lt;P&gt;I'm running Ubuntu 14.04 LTS 64 bit, I know it's not a "supported" version but perhaps this is still pertinent.&lt;/P&gt;&lt;P&gt;Just removing the file did not do the trick. I had to pass a --force-overwrite to dpkg as well.&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Unpacked the image by adding a "--keep" option &amp;nbsp;as in&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;"sudo ./mcuxpressoide-10.0.0_344.x86_64.deb.bin &amp;nbsp;--keep"&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;this extracted the files into an "installer" sub dir&lt;/P&gt;&lt;P&gt;2. edited install.sh via:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;"sudo vi install.sh"&lt;/P&gt;&lt;P&gt;3. added the --force-overwrite &amp;nbsp;option to the dpkg command for the ide install as in:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;was originally: &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; dpkg -i --force-depends mcuxpressoide-10.0.0_344.x86_64.deb&lt;BR /&gt;&amp;nbsp; changed to&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;dpkg -i --force-depends --force-overwrite mcuxpressoide-10.0.0_344.x86_64.deb&lt;/P&gt;&lt;P&gt;&amp;nbsp;4. ran the install script via:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; "sudo ./install.sh"&amp;nbsp;&lt;/P&gt;&lt;P&gt;The ide has installed and did start up, at least the initial view.&lt;/P&gt;&lt;P&gt;Both kds and MCUxpresso ide are up in the initial view, not sure yet beyond this as I'm not planning to try to run them at the same time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Leroy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Mar 2017 19:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615440#M20</guid>
      <dc:creator>leroyle</dc:creator>
      <dc:date>2017-03-27T19:53:06Z</dc:date>
    </item>
    <item>
      <title>Re: Running KDS 3.2 alongside MCUXpresso on Linux</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615441#M21</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Leroy,&lt;/P&gt;&lt;P&gt;sorry, yes you are right, removing the file won't do the trick. Your procedure will :smileywink: Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Zdar&lt;/P&gt;&lt;P&gt;MCUXpresso support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 12:03:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Running-KDS-3-2-alongside-MCUXpresso-on-Linux/m-p/615441#M21</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2017-03-28T12:03:39Z</dc:date>
    </item>
  </channel>
</rss>