<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso General中的主题 Re: Place slave code in Flash memory LPC55S69</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918631#M2051</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Neculai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late replay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I finally found how this is done. Please check the instructions bellow:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First you will need to create the SLAVE Project. In the Quickstart Panel select the option New Project, select the SDK from the LPC5556x. In the next window select the option for Slave core:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86156iA21C31D2A73D74E6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Press the next button and in the next window, split the flash memory and delete the first and third RAM&amp;nbsp;section. Also in the driver for the flash controller select the LPC55xx_S.cfx. After that press the Finish button&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86229iD5484A937C2D6201/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You'll need to create now the master core project. Follow the same process and in the next window select the option for master core:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86330iF085DE96FE39D7DA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the following window split the flash memory, and select in the Slave project for M33Slave the project you previously create. Doesn't matter the Link section since we'll change it. Also the driver leave it as it is. Press the finish button.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86371iC899561712293698/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After that, we'll need to set the second flash section as the one used for the slave core. Access to the properties of the project -&amp;gt; C/C++ Build -&amp;gt; Settings -&amp;gt;MCU Linker -&amp;gt; Multicore and in the Master Memory select the second section of the flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86413iE47C2C609579B84C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_9.png" alt="pastedImage_9.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After that, always start the debug session of the master core and after the second core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Aug 2019 17:44:39 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2019-08-07T17:44:39Z</dc:date>
    <item>
      <title>Place slave code in Flash memory LPC55S69</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918627#M2047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the LPC55S69-EVK development board (LPCXpresso55S69) and IDE V11.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I place the slave code in flash memory using the "New Project ..." command?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In this way, to create a new master / slave project, the IDE places the slave executable code in SRAMX without the option of being placed in Flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you solve this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Neculai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 30 Jun 2019 17:50:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918627#M2047</guid>
      <dc:creator>naga</dc:creator>
      <dc:date>2019-06-30T17:50:11Z</dc:date>
    </item>
    <item>
      <title>Re: Place slave code in Flash memory LPC55S69</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918628#M2048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Neculai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The image of the slave code is placed in RAM but the primary code will boot the secondary core and place the image in flash.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/90425i5A84FDB63F681FCD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If you check the .map file you can see something like this that says where is loaded the slave core image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jul 2019 01:38:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918628#M2048</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-07-05T01:38:16Z</dc:date>
    </item>
    <item>
      <title>Re: Place slave code in Flash memory LPC55S69</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918629#M2049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You should be able to do this if you split the flash available on this device into two "partitions" using the IDE's Memory Configuration Editor. You will then need to ensure that the master and the slave projects list the appropriate flash partition first in their memory configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However doing so is definitely not going to be good from a performance point of view, as you will get bus contention from the two cores both trying to access the flash at the same time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 13:58:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918629#M2049</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-07-09T13:58:13Z</dc:date>
    </item>
    <item>
      <title>Re: Place slave code in Flash memory LPC55S69</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918630#M2050</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Placing the code in SRAM or Flash memory involves advantages and disadvantages in each case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To make a brief presentation, I only add a few disadvantages of placing the code in SRAM:&lt;BR /&gt;- Memory space is simultaneously used, with the same code in SRAM and Flash&lt;BR /&gt;- An electromagnetic pulse can alter the executable code information in SRAM that is only restored to a new reset.&lt;BR /&gt;- The size of the executable code is limited to the SRAMX size&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;These are the reasons why I want to place both master / slave codes in Flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The "LPC55S6x product data sheet" document should specify power consumption performance and computing performance when both cores are active and work at 12, 48 and 96 MHz frequencies, similar to the tables&lt;BR /&gt;- Table 15. CoreMark score,&lt;BR /&gt;- Table 16. Static characteristics: Power consumption in active and sleep modes,&lt;BR /&gt;- Table 16 next. Static characteristics: Power consumption in active and sleep modes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The expression "not going to be good from a performance point of view" is relative, while design engineers need absolute data.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I'm interested in what exactly are the steps to be taken in case of a new dual core project in IDE so that the codes are placed exclusively in Flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Neculai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 19:07:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918630#M2050</guid>
      <dc:creator>naga</dc:creator>
      <dc:date>2019-07-09T19:07:20Z</dc:date>
    </item>
    <item>
      <title>Re: Place slave code in Flash memory LPC55S69</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918631#M2051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Neculai,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late replay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I finally found how this is done. Please check the instructions bellow:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First you will need to create the SLAVE Project. In the Quickstart Panel select the option New Project, select the SDK from the LPC5556x. In the next window select the option for Slave core:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86156iA21C31D2A73D74E6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Press the next button and in the next window, split the flash memory and delete the first and third RAM&amp;nbsp;section. Also in the driver for the flash controller select the LPC55xx_S.cfx. After that press the Finish button&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86229iD5484A937C2D6201/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You'll need to create now the master core project. Follow the same process and in the next window select the option for master core:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86330iF085DE96FE39D7DA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the following window split the flash memory, and select in the Slave project for M33Slave the project you previously create. Doesn't matter the Link section since we'll change it. Also the driver leave it as it is. Press the finish button.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86371iC899561712293698/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;After that, we'll need to set the second flash section as the one used for the slave core. Access to the properties of the project -&amp;gt; C/C++ Build -&amp;gt; Settings -&amp;gt;MCU Linker -&amp;gt; Multicore and in the Master Memory select the second section of the flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86413iE47C2C609579B84C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_9.png" alt="pastedImage_9.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After that, always start the debug session of the master core and after the second core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2019 17:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Place-slave-code-in-Flash-memory-LPC55S69/m-p/918631#M2051</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-08-07T17:44:39Z</dc:date>
    </item>
  </channel>
</rss>