<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso General中的主题 Re: LPC17xx - Cannot halt process issue</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/LPC17xx-Cannot-halt-process-issue/m-p/911834#M1976</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marco,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What happens when you try to boot into ISP mode? Does it enters successfully into ISP mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Aug 2019 17:58:33 GMT</pubDate>
    <dc:creator>FelipeGarcia</dc:creator>
    <dc:date>2019-08-28T17:58:33Z</dc:date>
    <item>
      <title>LPC17xx - Cannot halt process issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC17xx-Cannot-halt-process-issue/m-p/911833#M1975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm stuck with a "Cannot halt process" issue while trying to program a LPC17xx MCU on a custom board. I've loaded in debug mode several time the same project without any problem, but at a certain point it stopped working and I can't program che chip anymore. I've tried to follow the instructions about&amp;nbsp;&lt;A href="https://community.nxp.com/thread/389112"&gt;Regaining debug access to target MCU&lt;/A&gt;&amp;nbsp;, but unfortunately I still can't access the chip in any mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also tried to erase the Flash memory from "Debug configuration" window, but it gave me back the same error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This are the console messages when I&amp;nbsp;launch the debug:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;MCUXpresso IDE RedlinkMulti Driver v10.2 (Jul 25 2018 11:25:37 - crt_emu_cm_redlink build 555)&lt;BR /&gt;Reconnected to existing link server&lt;BR /&gt;Connecting to probe 1 core 0:0 (using server started externally) gave 'OK'&lt;BR /&gt;Probe Firmware: LPC-Link Probe v1.3 (NXP - LPC-Link)&lt;BR /&gt;Serial Number: HID64HS12&lt;BR /&gt;VID:PID: 1FC9:0007&lt;BR /&gt;USB Path:&lt;BR /&gt;Using memory from core 0:0 after searching for a good core&lt;BR /&gt;debug interface type = Cortex-M3/4 (DAP DP ID 2BA01477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M3 (CPU ID 00000C23) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 6&lt;BR /&gt;number of flash patches = 2&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 2BA01477. CpuID: 00000C23. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FF000: CID B105100D PID 0000000000 ROM dev (type 0x1)&lt;BR /&gt;ROM 1 E000E000: CID B105E00D PID 04002BB000 ChipIP dev SCS (type 0x0)&lt;BR /&gt;ROM 1 E0001000: CID B105E00D PID 04002BB002 ChipIP dev DWT (type 0x0)&lt;BR /&gt;ROM 1 E0002000: CID B105E00D PID 04002BB003 ChipIP dev FPB (type 0x0)&lt;BR /&gt;ROM 1 E0000000: CID B105E00D PID 04002BB001 ChipIP dev ITM (type 0x0)&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04002BB923 CoreSight dev TPIU-Lite type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0041000: CID B105900D PID 04002BB924 CoreSight dev ETM-M3 type 0x13 Trace Source - core&lt;BR /&gt;Cannot halt processor&lt;BR /&gt;&lt;STRONG&gt;Failed on chip setup: Ep(04). Cannot halt processor.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm pretty sure that the loaded project didn't block access to Flash memory in any way.&lt;/P&gt;&lt;P&gt;What can I do to program the MCU again?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance, best regards.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 13:45:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC17xx-Cannot-halt-process-issue/m-p/911833#M1975</guid>
      <dc:creator>software3</dc:creator>
      <dc:date>2019-08-27T13:45:28Z</dc:date>
    </item>
    <item>
      <title>Re: LPC17xx - Cannot halt process issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC17xx-Cannot-halt-process-issue/m-p/911834#M1976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Marco,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What happens when you try to boot into ISP mode? Does it enters successfully into ISP mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 17:58:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC17xx-Cannot-halt-process-issue/m-p/911834#M1976</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-08-28T17:58:33Z</dc:date>
    </item>
  </channel>
</rss>