<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debugger terminates unexpectedly in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904349#M1906</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Harald,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will suggest to&amp;nbsp;reconfigure the libraries to build using Newlib rather than Redlib. Also check the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://isocpp.org/wiki/faq/mixing-c-and-cpp#call-cpp"&gt;https://isocpp.org/wiki/faq/mixing-c-and-cpp#call-cpp&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There's some suggestions about to mix C/C++ code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 May 2019 19:49:34 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2019-05-13T19:49:34Z</dc:date>
    <item>
      <title>Debugger terminates unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904345#M1902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;so after just having solved my debugger startup problems, the next item appears.&lt;/P&gt;&lt;P&gt;In general, the effect is that the debugger terminates after inserting a breakpoint and resuming the operation.&lt;/P&gt;&lt;P&gt;The application had run before a good time, so to say it is not the application that causes the termination.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The thing is that I have a FreeRTOS application with mixed C and C++ code.&lt;/P&gt;&lt;P&gt;The debugger termination only happens if you set the breakpoint in a pure C file (e.g. event_groups.c)&lt;/P&gt;&lt;P&gt;The application doesn't continue but I cannot say where it is stuck.&lt;/P&gt;&lt;P&gt;Any ideas to that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for supporting in advance - Harald.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2019 19:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904345#M1902</guid>
      <dc:creator>haraldadolph</dc:creator>
      <dc:date>2019-05-07T19:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger terminates unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904346#M1903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Haraid,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you let me know which MCU and which debugger are you using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2019 16:41:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904346#M1903</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-05-10T16:41:37Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger terminates unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904347#M1904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Alexis, sorry for the missing details.&lt;/P&gt;&lt;P&gt;I'm using K66 - 180 with McuXPresso / P&amp;amp;E debugger. I have tried both versions of the debugger (standard and FX), it's the same behaviour in any case.&lt;/P&gt;&lt;P&gt;Unfortunately, it is not possible to debug the behaviour of the events being set from ISR - they happen to work but not in any case, so to find the cause is very hard.&lt;/P&gt;&lt;P&gt;Do you have any similar experience?&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Harald.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 05:45:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904347#M1904</guid>
      <dc:creator>haraldadolph</dc:creator>
      <dc:date>2019-05-13T05:45:32Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger terminates unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904348#M1905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexis. &lt;/P&gt;&lt;P&gt;Another - maybe important - item I did not mention up to now is that the program runs without debugger - as far as I can say that. The problem I want to debug is based in the event handling - and as I said I haven't the possibility to debug as the event comes from an ISR. The event handling is handed over to the Tmr SVC task, and to set a break there terminates the software and the debugger immediately.&lt;/P&gt;&lt;P&gt;Greetings Harald.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 19:42:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904348#M1905</guid>
      <dc:creator>haraldadolph</dc:creator>
      <dc:date>2019-05-13T19:42:05Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger terminates unexpectedly</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904349#M1906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Harald,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will suggest to&amp;nbsp;reconfigure the libraries to build using Newlib rather than Redlib. Also check the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://isocpp.org/wiki/faq/mixing-c-and-cpp#call-cpp"&gt;https://isocpp.org/wiki/faq/mixing-c-and-cpp#call-cpp&lt;/A&gt;&lt;/P&gt;&lt;P&gt;There's some suggestions about to mix C/C++ code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 19:49:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugger-terminates-unexpectedly/m-p/904349#M1906</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-05-13T19:49:34Z</dc:date>
    </item>
  </channel>
</rss>