<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Some problem for SDK Demo(board KL25Z) in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Some-problem-for-SDK-Demo-board-KL25Z/m-p/902483#M1901</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, the readme is puzzling. There is nothing to do with UART0 and J20. The example use UART1 and openSDA VCOM channel. Maybe the person who make the SDK used wrong file. I'll report this problem.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Apr 2019 09:27:01 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2019-04-22T09:27:01Z</dc:date>
    <item>
      <title>Some problem for SDK Demo(board KL25Z)</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Some-problem-for-SDK-Demo-board-KL25Z/m-p/902482#M1900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to run a UART demo for KL25Z with MCUXPesso IDE. I import a uart demo from SDK, the docs(readme.txt) of project show as follow:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board settings&lt;BR /&gt;==============&lt;BR /&gt;The connection should be set as following:&lt;BR /&gt;- RX of USB2COM connected to J2-18&lt;BR /&gt;- TX of USB2COM connected to J2-20&lt;BR /&gt;- GND of USB2COM connected to J2-14&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;according to board settings, what i should do next? what i should to connect for the board???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 11:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Some-problem-for-SDK-Demo-board-KL25Z/m-p/902482#M1900</guid>
      <dc:creator>crj1998</dc:creator>
      <dc:date>2019-04-19T11:58:29Z</dc:date>
    </item>
    <item>
      <title>Re: Some problem for SDK Demo(board KL25Z)</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Some-problem-for-SDK-Demo-board-KL25Z/m-p/902483#M1901</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Yes, the readme is puzzling. There is nothing to do with UART0 and J20. The example use UART1 and openSDA VCOM channel. Maybe the person who make the SDK used wrong file. I'll report this problem.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Apr 2019 09:27:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Some-problem-for-SDK-Demo-board-KL25Z/m-p/902483#M1901</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-04-22T09:27:01Z</dc:date>
    </item>
  </channel>
</rss>