<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: spell checking freeze the complete development environment. in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899566#M1884</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;new tests:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;other PC with windows 10, 64 bit with SSD &lt;BR /&gt;i have cut the LAN Kbael and deaktivate all virus scanners.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the same problem&lt;BR /&gt;ca. 4-5 secounds before the source code changed in the editor window....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tested with:&lt;BR /&gt;MCUXpresso IDE v10.2.1 [Build 795] [2018-07-25] &lt;BR /&gt;MCUXpresso IDE v10.3.1 [Build 2233] [2019-02-20]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i cant normal work if spell cheking is on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;the 4th PC with the same problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;new installation of the old version LPCXpresso &lt;/P&gt;&lt;P&gt;there is also the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Siro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Apr 2019 16:43:47 GMT</pubDate>
    <dc:creator>berndsirozynski</dc:creator>
    <dc:date>2019-04-17T16:43:47Z</dc:date>
    <item>
      <title>spell checking freeze the complete development environment.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899563#M1881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if i enable the spell checking, which is the default on mcuxpresso. (which is nonsnes for a programming language :-) &lt;BR /&gt;every change in my source code needs to 10 secounds before it updated on the screen.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this problem occurs only on big source files.&lt;BR /&gt;in my situation the source is over 5000 Lines&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;maybe it is a problem of Eclipse ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This problem was found in MCUXpresso V3.0 and V3.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Siro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 10:30:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899563#M1881</guid>
      <dc:creator>berndsirozynski</dc:creator>
      <dc:date>2019-04-17T10:30:16Z</dc:date>
    </item>
    <item>
      <title>Re: spell checking freeze the complete development environment.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899564#M1882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Siro,&lt;/P&gt;&lt;P&gt;I don't see such a delay on my side, and I have source files with &amp;gt;10k LOC.&lt;/P&gt;&lt;P&gt;Are you using the default spelling engine?&lt;/P&gt;&lt;P&gt;Where do you have your user dictionalyr stored? Make sure it is on a low latency path (local machine disk) and not on a network path.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 11:09:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899564#M1882</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-04-17T11:09:28Z</dc:date>
    </item>
    <item>
      <title>Re: spell checking freeze the complete development environment.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899565#M1883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Erich,&lt;BR /&gt;thanks for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am only working on a "local" machine with Windows 7&lt;BR /&gt;on a normal(mechanical) Harddisk, no SSD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and did not install anything in addition, only the MCUXpresso from the NXP Website.&lt;BR /&gt;So, i think, the spell checking ist directly from this installed tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is now not a problem, because i dont want the spell check in a programming language,&lt;BR /&gt;but it need lot of time to find the reason.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;but wondering that you dont have this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will test it also at evening on my home PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Siro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 12:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899565#M1883</guid>
      <dc:creator>berndsirozynski</dc:creator>
      <dc:date>2019-04-17T12:21:28Z</dc:date>
    </item>
    <item>
      <title>Re: spell checking freeze the complete development environment.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899566#M1884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;BR /&gt;new tests:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;other PC with windows 10, 64 bit with SSD &lt;BR /&gt;i have cut the LAN Kbael and deaktivate all virus scanners.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the same problem&lt;BR /&gt;ca. 4-5 secounds before the source code changed in the editor window....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tested with:&lt;BR /&gt;MCUXpresso IDE v10.2.1 [Build 795] [2018-07-25] &lt;BR /&gt;MCUXpresso IDE v10.3.1 [Build 2233] [2019-02-20]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i cant normal work if spell cheking is on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;the 4th PC with the same problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;new installation of the old version LPCXpresso &lt;/P&gt;&lt;P&gt;there is also the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Siro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 16:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/spell-checking-freeze-the-complete-development-environment/m-p/899566#M1884</guid>
      <dc:creator>berndsirozynski</dc:creator>
      <dc:date>2019-04-17T16:43:47Z</dc:date>
    </item>
  </channel>
</rss>