<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックFTM input capture mode, CnV value</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/FTM-input-capture-mode-CnV-value/m-p/898292#M1846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using KV31F FTM1 ch1, FTM2 ch0, FTM3 ch1 as an input capture on both edges. The channels are generating interrupts, however the CnV value is only loading 0's. Is there a required command to start the CNT with input capture mode or a required way to read the Cnv?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see attached FTM1 ch1 Initialization code. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 May 2019 16:49:39 GMT</pubDate>
    <dc:creator>perryjagger</dc:creator>
    <dc:date>2019-05-01T16:49:39Z</dc:date>
    <item>
      <title>FTM input capture mode, CnV value</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/FTM-input-capture-mode-CnV-value/m-p/898292#M1846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using KV31F FTM1 ch1, FTM2 ch0, FTM3 ch1 as an input capture on both edges. The channels are generating interrupts, however the CnV value is only loading 0's. Is there a required command to start the CNT with input capture mode or a required way to read the Cnv?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see attached FTM1 ch1 Initialization code. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 May 2019 16:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/FTM-input-capture-mode-CnV-value/m-p/898292#M1846</guid>
      <dc:creator>perryjagger</dc:creator>
      <dc:date>2019-05-01T16:49:39Z</dc:date>
    </item>
    <item>
      <title>Re: FTM input capture mode, CnV value</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/FTM-input-capture-mode-CnV-value/m-p/898293#M1847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="340694" data-username="perryjagger" href="https://community.nxp.com/people/perryjagger"&gt;Perry Jagger&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I strongly recommend you first check the input capture demo under MCUXpresso SDK.&lt;/P&gt;&lt;P&gt;Download from &lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/select" title="https://mcuxpresso.nxp.com/en/select"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80453i7A05F447D07C43F1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;it support MCUXpresso IDE, IAR and KEIL.&lt;/P&gt;&lt;P&gt;There is a demo named "ftm_input_capture" under "driver_examles" folder:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80496i64FE26C285266A12/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 May 2019 03:55:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/FTM-input-capture-mode-CnV-value/m-p/898293#M1847</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-05-06T03:55:00Z</dc:date>
    </item>
  </channel>
</rss>