<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: MCUXpresso setting lib include path</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-setting-lib-include-path/m-p/896502#M1836</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="336086" data-username="lschoenfeld@wezag.de" href="https://community.nxp.com/people/lschoenfeld@wezag.de"&gt;Lothar Schönfeld&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;- In your attachment , the path under "Includes" are the header files that project used, these can add directly in C/C++ Build -&amp;gt; Settings -&amp;gt; ....-&amp;gt; Includes as attachment "Includes.png".&lt;/P&gt;&lt;P&gt;- About add Library, please refer to this link: &lt;A href="https://community.nxp.com/thread/388991"&gt;Creating and Linking to Library Projects&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- In your project, it can include stdio.h, this is under redlib, from attachment I know you have includes this lib.&lt;/P&gt;&lt;P&gt;what about the error message?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 May 2019 08:43:13 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2019-05-16T08:43:13Z</dc:date>
    <item>
      <title>MCUXpresso setting lib include path</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-setting-lib-include-path/m-p/896501#M1835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working with the example project "bluetooth_otpa_client_freertos" for KW41Z and have to use some lib funktions included in stdio library. How can I set the lib path in MCUxpresso? As soon as I include stdio.h in source code it causes an error. In an other example "bluetooth_wireless_uart_freertos" the lib path was set automatic (see attachment).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Lothar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 04:53:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-setting-lib-include-path/m-p/896501#M1835</guid>
      <dc:creator>lschoenfeld</dc:creator>
      <dc:date>2019-05-16T04:53:26Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso setting lib include path</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-setting-lib-include-path/m-p/896502#M1836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="336086" data-username="lschoenfeld@wezag.de" href="https://community.nxp.com/people/lschoenfeld@wezag.de"&gt;Lothar Schönfeld&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;- In your attachment , the path under "Includes" are the header files that project used, these can add directly in C/C++ Build -&amp;gt; Settings -&amp;gt; ....-&amp;gt; Includes as attachment "Includes.png".&lt;/P&gt;&lt;P&gt;- About add Library, please refer to this link: &lt;A href="https://community.nxp.com/thread/388991"&gt;Creating and Linking to Library Projects&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- In your project, it can include stdio.h, this is under redlib, from attachment I know you have includes this lib.&lt;/P&gt;&lt;P&gt;what about the error message?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 08:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-setting-lib-include-path/m-p/896502#M1836</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-05-16T08:43:13Z</dc:date>
    </item>
  </channel>
</rss>