<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debug works only one time in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891444#M1764</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Finally found that I am not the only one who is being bothered by this problem. I have three LPCXpresso boards on hand:&lt;/P&gt;&lt;P&gt;* LPCXpresso LPC812 REV B&lt;/P&gt;&lt;P&gt;* LPCXpresso LPC1200 REV B&lt;/P&gt;&lt;P&gt;* LPCXpresso LPC812-MAX&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I am using the lastest MCUXpresso IDE verion - v11.0.1, the debug session can only run for one time on both LPC812 and LPC1200. I have to disconnect the USB calbe and connect it again if I want to start a new debug session.&lt;/P&gt;&lt;P&gt;But on LPC812-MAX (with a built-in CMSIS-DAP), I didn't find this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I installed LCPXpresso IDE v8.2.2,&amp;nbsp; found that debugging with LPC1200 and LPC812 works well. Seems MCUXpresso IDE has some issue or different configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Nov 2019 09:03:12 GMT</pubDate>
    <dc:creator>joelmiao</dc:creator>
    <dc:date>2019-11-27T09:03:12Z</dc:date>
    <item>
      <title>Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891438#M1758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i used the MCUXpresso IDE 3.1 and the LPC-Link Board for the LPC1768&lt;/P&gt;&lt;P&gt;I can only Debug a Program one time.&lt;/P&gt;&lt;P&gt;If i change my Source and want to debug again,&lt;/P&gt;&lt;P&gt;i get errors. cant connect.....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To solve the problem:&lt;/P&gt;&lt;P&gt;a) i must close the complete IDE and Start again.&lt;/P&gt;&lt;P&gt;b) i must disconnect the USB from the LPC Link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, i have deinstalled the complete IDE and reinstalled&lt;/P&gt;&lt;P&gt;The same problem again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, i have&amp;nbsp; istalled the previous version 3.0&lt;/P&gt;&lt;P&gt;and all works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Siro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2019 09:54:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891438#M1758</guid>
      <dc:creator>berndsirozynski</dc:creator>
      <dc:date>2019-04-10T09:54:36Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891439#M1759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello again,&lt;/P&gt;&lt;P&gt;now i have tried to install the IDE the 3rd time. to inform you about the error mesages&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;if i stop my debug session&lt;BR /&gt;next debugging doesnt work and shows 3 error Windows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;----------------&lt;BR /&gt;Windows 1: Error reported by target&lt;BR /&gt;02: Failed on connect&lt;BR /&gt;Could not connect to core.&lt;BR /&gt;31: No connection to chips's debug port&lt;BR /&gt;Debugging contexte: project1 LinkServer Debug&lt;BR /&gt;----------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Window2: LinkServer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;17^error,msg?"Remote communication error. Target disconnected,: Success."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reason: &lt;BR /&gt;Failed to execute MI command:&lt;BR /&gt;-target-select extended-remote | crt_emu_cm_redlink -msg-port=49873 -g -mi -2&lt;BR /&gt;-pLPC1768 -vendor=NXP&amp;nbsp; --reset=VECTRESET -ProbeHandle=1 -CorIndex=0&lt;BR /&gt;--flash-driver LPC175x_6x_512.cfx --telnet 3330&lt;BR /&gt;Error message from debugger back end_&lt;BR /&gt;Remote communication error. Target disconnetcted.: Success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;----------------&lt;BR /&gt;Window 3:&amp;nbsp; Problem Occured&lt;BR /&gt;'Launching project1 LinkServer Debug' has encountered a &lt;BR /&gt;problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Error in final launch sequence&lt;BR /&gt;&amp;nbsp; Failed to execute MI command:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;----------------&lt;BR /&gt;Consolen output:&lt;BR /&gt;MCUXpresso IDE RedlinkMulti Driver v10.3 (Feb&amp;nbsp; 7 2019 22:50:02 - crt_emu_cm_redlink build 760)&lt;BR /&gt;Found part description in XML file nxp_lpc17xx.xme&lt;BR /&gt;(&amp;nbsp; 5) Remote configuration complete&lt;BR /&gt;Reconnected to existing link server&lt;BR /&gt;Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'&lt;BR /&gt;Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'&lt;BR /&gt;Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'&lt;BR /&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port&lt;BR /&gt;------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Button "Clean Up Debug" dont change the behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;a next test with another project has the same results.&lt;/P&gt;&lt;P&gt;i cant locate the problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debugging all projects with the MCUXPresso IDE Version 3.0 has no problems&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Siro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2019 07:14:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891439#M1759</guid>
      <dc:creator>berndsirozynski</dc:creator>
      <dc:date>2019-04-11T07:14:27Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891440#M1760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;never give up,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so i have a complete other Windows PC and installed followed versions:&lt;BR /&gt;also i have a new LPC-Link and also i have a minimum Hardware only the LPC1768xx on my Board &lt;BR /&gt;connected with SWD&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXPresso V10.2.1 all work fine&lt;BR /&gt;MCUXpresso V10.3.1 has identical problems with debugging&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so, it is better to work with an older version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Siro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2019 16:47:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891440#M1760</guid>
      <dc:creator>berndsirozynski</dc:creator>
      <dc:date>2019-04-11T16:47:35Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891441#M1761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i have found the problem:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Version MCUXpresso Version V10.3.1 has only Problems with the&lt;/P&gt;&lt;P&gt;LPC-Link (Breakout Board from LPCXpresso Board LPC1769)&lt;/P&gt;&lt;P&gt;with the a New LPC-LINK 2 board, there is no problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Very Happy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 12:20:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891441#M1761</guid>
      <dc:creator>berndsirozynski</dc:creator>
      <dc:date>2019-04-15T12:20:48Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891442#M1762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Bernd,&lt;/P&gt;&lt;P&gt;Thanks for your sharing.&lt;/P&gt;&lt;P&gt;I will report it to development team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 09:38:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891442#M1762</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-04-18T09:38:40Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891443#M1763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am having this same problem with MCUXpresso IDE 11.0 and LPC845Max board.&amp;nbsp; Trying to run Multi-Timer Blinky example.&amp;nbsp; If I run it under the LinkServer debugger the first time after powering up the board, it runs fine.&amp;nbsp; If I terminate the debug, then restart it again, it fails the 2nd time with the same errors described above.&amp;nbsp;&amp;nbsp; If I unplug the board from USB and then reconnect, the debugger works again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 18:56:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891443#M1763</guid>
      <dc:creator>kk7xo</dc:creator>
      <dc:date>2019-08-22T18:56:47Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891444#M1764</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Finally found that I am not the only one who is being bothered by this problem. I have three LPCXpresso boards on hand:&lt;/P&gt;&lt;P&gt;* LPCXpresso LPC812 REV B&lt;/P&gt;&lt;P&gt;* LPCXpresso LPC1200 REV B&lt;/P&gt;&lt;P&gt;* LPCXpresso LPC812-MAX&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I am using the lastest MCUXpresso IDE verion - v11.0.1, the debug session can only run for one time on both LPC812 and LPC1200. I have to disconnect the USB calbe and connect it again if I want to start a new debug session.&lt;/P&gt;&lt;P&gt;But on LPC812-MAX (with a built-in CMSIS-DAP), I didn't find this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I installed LCPXpresso IDE v8.2.2,&amp;nbsp; found that debugging with LPC1200 and LPC812 works well. Seems MCUXpresso IDE has some issue or different configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 09:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/891444#M1764</guid>
      <dc:creator>joelmiao</dc:creator>
      <dc:date>2019-11-27T09:03:12Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1602635#M4856</link>
      <description>I have the same problem as yours. My MCUXpresso version is 11.6.1. feel frustrated.</description>
      <pubDate>Tue, 21 Feb 2023 07:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1602635#M4856</guid>
      <dc:creator>wangwenyu</dc:creator>
      <dc:date>2023-02-21T07:54:56Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1602703#M4857</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206964"&gt;@wangwenyu&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;could you share what board you are using, just in case?&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Tue, 21 Feb 2023 08:48:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1602703#M4857</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-02-21T08:48:12Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1602992#M4858</link>
      <description>&lt;P&gt;I use MCUXpresso to connect my target board through a MCU-Link pro. The target board is a simple system on which a LPC11U68 connects a NTAG plus chip through IIC. The ROM driver is used.&lt;/P&gt;&lt;P&gt;It works properly at the first time when I debug this board. But, after I repower the target board, the MCUXpresso never connects with the target board again. This problem continuously occured on my 5 boards. The first time always works. Then the MCUXpresso never connects the target again.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wangwenyu_0-1676989745807.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/211813i526EA765CE80A328/image-size/medium?v=v2&amp;amp;px=400" role="button" title="wangwenyu_0-1676989745807.png" alt="wangwenyu_0-1676989745807.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;wangwenyu_0-1676989745807.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is highly appreciated if some body help me.&lt;/P&gt;&lt;P&gt;I have struggled for 4 days. No clue is found.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Feb 2023 14:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1602992#M4858</guid>
      <dc:creator>wangwenyu</dc:creator>
      <dc:date>2023-02-21T14:30:48Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1602995#M4859</link>
      <description>The below is my information. If you can help me, please. Thanks.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-can-t-access-the-lpc11u68-after-the-first-time-of/m-p/1602627#M8770" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-can-t-access-the-lpc11u68-after-the-first-time-of/m-p/1602627#M8770&lt;/A&gt;&lt;BR /&gt;</description>
      <pubDate>Tue, 21 Feb 2023 14:31:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1602995#M4859</guid>
      <dc:creator>wangwenyu</dc:creator>
      <dc:date>2023-02-21T14:31:53Z</dc:date>
    </item>
    <item>
      <title>Re: Debug works only one time</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1790358#M5293</link>
      <description>&lt;P&gt;I have this problem with v11.8.1 on my Thinkpad laptop, but my desktop is fine with the same version!&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 13:54:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-works-only-one-time/m-p/1790358#M5293</guid>
      <dc:creator>Bariel76</dc:creator>
      <dc:date>2024-01-17T13:54:41Z</dc:date>
    </item>
  </channel>
</rss>