<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックProblem with MCU Bootloader 2.0.0 and update with USB-HID interface</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Problem-with-MCU-Bootloader-2-0-0-and-update-with-USB-HID/m-p/883148#M1660</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I’m using MCU Bootloader 2.0.0 and KinetisFlashTool with FRDM-K64F. I followed the steps to test the Bootloader and KinetisFlashTool as described in MCU Bootloader Demo Applications User's Guide (Document Number: MBOOTDEMOUG).&lt;/P&gt;&lt;P&gt;After loading the Bootloader to the device (through OpenSDA) I was able to use KinetisFlashTool and update the application using UART Port set in KinetisFlashTool. Using UART Port, I see that the blhost works as expected.&lt;/P&gt;&lt;P&gt;To update the application through USB-HID, I used the K64F USB port on board (J22) and set the Port in KinetisFlashTool to USB-HID. The BCA area in the application was updated to prepare both UART and USB peripherals as shown in the attached snapshot.&lt;/P&gt;&lt;P&gt;Unfortunately, no connection is made through the USB port, see the error message in the attached snapshot.&lt;/P&gt;&lt;P&gt;Error: Connect device failed(Error: UsbHidPeripheral() cannot open USB HID device (vid=0x15a2, pid=0x0073, sn=).).&lt;/P&gt;&lt;P&gt;The USB connection is not even in the Device Manager.&lt;/P&gt;&lt;P&gt;Am I missing anything to do before using the USB-HID to update the application using Bootloader?&lt;/P&gt;&lt;P&gt;Should I make any changes in the Bootloader project to prepare it for a USB-HID update?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated!&lt;/P&gt;&lt;P&gt;Abi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Jan 2019 18:37:54 GMT</pubDate>
    <dc:creator>atfarsoni</dc:creator>
    <dc:date>2019-01-17T18:37:54Z</dc:date>
    <item>
      <title>Problem with MCU Bootloader 2.0.0 and update with USB-HID interface</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problem-with-MCU-Bootloader-2-0-0-and-update-with-USB-HID/m-p/883148#M1660</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I’m using MCU Bootloader 2.0.0 and KinetisFlashTool with FRDM-K64F. I followed the steps to test the Bootloader and KinetisFlashTool as described in MCU Bootloader Demo Applications User's Guide (Document Number: MBOOTDEMOUG).&lt;/P&gt;&lt;P&gt;After loading the Bootloader to the device (through OpenSDA) I was able to use KinetisFlashTool and update the application using UART Port set in KinetisFlashTool. Using UART Port, I see that the blhost works as expected.&lt;/P&gt;&lt;P&gt;To update the application through USB-HID, I used the K64F USB port on board (J22) and set the Port in KinetisFlashTool to USB-HID. The BCA area in the application was updated to prepare both UART and USB peripherals as shown in the attached snapshot.&lt;/P&gt;&lt;P&gt;Unfortunately, no connection is made through the USB port, see the error message in the attached snapshot.&lt;/P&gt;&lt;P&gt;Error: Connect device failed(Error: UsbHidPeripheral() cannot open USB HID device (vid=0x15a2, pid=0x0073, sn=).).&lt;/P&gt;&lt;P&gt;The USB connection is not even in the Device Manager.&lt;/P&gt;&lt;P&gt;Am I missing anything to do before using the USB-HID to update the application using Bootloader?&lt;/P&gt;&lt;P&gt;Should I make any changes in the Bootloader project to prepare it for a USB-HID update?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be appreciated!&lt;/P&gt;&lt;P&gt;Abi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 18:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problem-with-MCU-Bootloader-2-0-0-and-update-with-USB-HID/m-p/883148#M1660</guid>
      <dc:creator>atfarsoni</dc:creator>
      <dc:date>2019-01-17T18:37:54Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with MCU Bootloader 2.0.0 and update with USB-HID interface</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problem-with-MCU-Bootloader-2-0-0-and-update-with-USB-HID/m-p/883149#M1661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Abi Farsoni,&lt;/P&gt;&lt;P&gt;Since you use FRDM-K64F, you can download freedom_bootloader project in target/K64F12 directly. You don't need to change anything. Please check if windows has found K64 HID.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63637i3264A4E37A8C566C/image-size/large?v=v2&amp;amp;px=999" title="USB_HID.png" alt="USB_HID.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 03:34:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problem-with-MCU-Bootloader-2-0-0-and-update-with-USB-HID/m-p/883149#M1661</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-01-18T03:34:14Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with MCU Bootloader 2.0.0 and update with USB-HID interface</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problem-with-MCU-Bootloader-2-0-0-and-update-with-USB-HID/m-p/883150#M1662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you, Jing.&lt;/P&gt;&lt;P&gt;It works today, but the device name in the Device Manager is different (it is not vendor-defined device, see below). Any reason for this difference?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63796i2EF9AD9BEBAF2040/image-size/large?v=v2&amp;amp;px=999" title="dm.png" alt="dm.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 17:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problem-with-MCU-Bootloader-2-0-0-and-update-with-USB-HID/m-p/883150#M1662</guid>
      <dc:creator>atfarsoni</dc:creator>
      <dc:date>2019-01-18T17:26:49Z</dc:date>
    </item>
  </channel>
</rss>