<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Max14830 No data received. in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Max14830-No-data-received/m-p/882987#M1658</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;BR /&gt;I'm having trouble setting max14830 using ti dsp 28377 spi.&lt;BR /&gt;Spi_Write (0x9f, 0xce); // Global command operation&lt;BR /&gt;Spi_Write (0x05,0xFF); // Read revision number FF is filled in digits&lt;BR /&gt;Spi_Write (0x9f, 0xcd); // Global command not working&lt;BR /&gt;I confirmed the revision ID (= 0xB4) with the above command.&lt;/P&gt;&lt;P&gt;Next, Uart3 is set as follows.&lt;BR /&gt;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1b | 0x80,0x40); // [6] set1 to disable CLK&lt;BR /&gt;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1e | 0x80,0x88); // no RTS PLLBypass no PLLEn Ex Clock&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1c | 0x80,0x09); // DVILSB&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1d | 0x80,0x00); // DVIMSB&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x09 | 0x80,0x88); // tx mode1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x0A | 0x80,0x00); // tx mode1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x0b | 0x80,0x03); // 8bit length&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1b | 0x80,0x2c); // enable CLK, set x4 mode&lt;/P&gt;&lt;P&gt;Then, RX-TX is connected to the outside, and '0xAA' is input to TX and RX data is read but '0x3E' is read.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;Spi_Write (0x03 &amp;lt;&amp;lt; 5 | 0x80,0xAA);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;Spi_Write (0x03 &amp;lt;&amp;lt; 5,0x00);&lt;BR /&gt;How do I know if I can read RX data normally?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Mar 2019 05:33:27 GMT</pubDate>
    <dc:creator>poorand</dc:creator>
    <dc:date>2019-03-11T05:33:27Z</dc:date>
    <item>
      <title>Max14830 No data received.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Max14830-No-data-received/m-p/882987#M1658</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;BR /&gt;I'm having trouble setting max14830 using ti dsp 28377 spi.&lt;BR /&gt;Spi_Write (0x9f, 0xce); // Global command operation&lt;BR /&gt;Spi_Write (0x05,0xFF); // Read revision number FF is filled in digits&lt;BR /&gt;Spi_Write (0x9f, 0xcd); // Global command not working&lt;BR /&gt;I confirmed the revision ID (= 0xB4) with the above command.&lt;/P&gt;&lt;P&gt;Next, Uart3 is set as follows.&lt;BR /&gt;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1b | 0x80,0x40); // [6] set1 to disable CLK&lt;BR /&gt;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1e | 0x80,0x88); // no RTS PLLBypass no PLLEn Ex Clock&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1c | 0x80,0x09); // DVILSB&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1d | 0x80,0x00); // DVIMSB&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x09 | 0x80,0x88); // tx mode1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x0A | 0x80,0x00); // tx mode1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x0b | 0x80,0x03); // 8bit length&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Spi_Write ((port &amp;lt;&amp;lt; 5) | 0x1b | 0x80,0x2c); // enable CLK, set x4 mode&lt;/P&gt;&lt;P&gt;Then, RX-TX is connected to the outside, and '0xAA' is input to TX and RX data is read but '0x3E' is read.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;Spi_Write (0x03 &amp;lt;&amp;lt; 5 | 0x80,0xAA);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;Spi_Write (0x03 &amp;lt;&amp;lt; 5,0x00);&lt;BR /&gt;How do I know if I can read RX data normally?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 05:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Max14830-No-data-received/m-p/882987#M1658</guid>
      <dc:creator>poorand</dc:creator>
      <dc:date>2019-03-11T05:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: Max14830 No data received.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Max14830-No-data-received/m-p/882988#M1659</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lee&lt;/P&gt;&lt;P&gt;TMS320F28377 is not NXP product but TI. &lt;/P&gt;&lt;P&gt;Please contact TI support for its questions. Thanks.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://e2e.ti.com/" title="https://e2e.ti.com/"&gt;TI E2E Community&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 07:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Max14830-No-data-received/m-p/882988#M1659</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-03-11T07:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: Max14830 No data received.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Max14830-No-data-received/m-p/1317847#M4273</link>
      <description>&lt;P&gt;have you been able to fix this problem?&lt;/P&gt;</description>
      <pubDate>Wed, 04 Aug 2021 06:38:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Max14830-No-data-received/m-p/1317847#M4273</guid>
      <dc:creator>JVis</dc:creator>
      <dc:date>2021-08-04T06:38:50Z</dc:date>
    </item>
  </channel>
</rss>