<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Update LCD error, cannot connect through open SDA in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Update-LCD-error-cannot-connect-through-open-SDA/m-p/869539#M1499</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a problem to connect the MCUXpresso debugger to my KL46 Freedom board through the open SDA port. I use MCUXpresso 10.3. When I try to make a debug configuration I get always an error message (see picture in attachment). When I use the "Debug with PEMicro probes" button in the "Debug your project" windows, MCUXpresso don't found my board even I can see it mounted like a disk on my PC (I see it in&amp;nbsp;the device manager too). When I go to another PC all is going well with the same board. I have re-install the PEMicro driver, I have re-install MCUXpresso and the same problem is still there... An idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Jan 2019 10:14:07 GMT</pubDate>
    <dc:creator>sergemonnerat</dc:creator>
    <dc:date>2019-01-29T10:14:07Z</dc:date>
    <item>
      <title>Update LCD error, cannot connect through open SDA</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Update-LCD-error-cannot-connect-through-open-SDA/m-p/869539#M1499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a problem to connect the MCUXpresso debugger to my KL46 Freedom board through the open SDA port. I use MCUXpresso 10.3. When I try to make a debug configuration I get always an error message (see picture in attachment). When I use the "Debug with PEMicro probes" button in the "Debug your project" windows, MCUXpresso don't found my board even I can see it mounted like a disk on my PC (I see it in&amp;nbsp;the device manager too). When I go to another PC all is going well with the same board. I have re-install the PEMicro driver, I have re-install MCUXpresso and the same problem is still there... An idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 10:14:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Update-LCD-error-cannot-connect-through-open-SDA/m-p/869539#M1499</guid>
      <dc:creator>sergemonnerat</dc:creator>
      <dc:date>2019-01-29T10:14:07Z</dc:date>
    </item>
    <item>
      <title>Re: Update LCD error, cannot connect through open SDA</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Update-LCD-error-cannot-connect-through-open-SDA/m-p/869540#M1500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you share a screenshot of your debugger launch configuration?&lt;/P&gt;&lt;P&gt;Check the project name and the C/C++ Application settings (marked below):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/30308i4B9E55411585C4B3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I think you have them somehow empty or wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 11:35:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Update-LCD-error-cannot-connect-through-open-SDA/m-p/869540#M1500</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-01-29T11:35:34Z</dc:date>
    </item>
  </channel>
</rss>