<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso General中的主题 Re: RT105x USB BC support</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/RT105x-USB-BC-support/m-p/869377#M1496</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mateusz Piesta&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;or maybe USB stack is not yet prepared for BC support on RT1051 ?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;USBDCD is not in RT1050, this is why the FSL_FEATURE_SOC_USBDCD_COUNT is cero, in the RT1050 devices you can find the&amp;nbsp;USB_ANALOG in the USB-PHY part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This Phy is capable of the charger detection which &lt;EM&gt;"detects whether the upstream-facing device is connected to a down-stream facing charger, either a dedicated USB charger or a host charger". &lt;/EM&gt;Unfortunately, this is not implemented in the usb_phy.c file of the USB stack, so the customer would need to add it&lt;EM&gt;. &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Feb 2019 01:06:28 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2019-02-01T01:06:28Z</dc:date>
    <item>
      <title>RT105x USB BC support</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/RT105x-USB-BC-support/m-p/869376#M1495</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are designing custom device based on RT1051 uC which is battery powered. We need to have option for charging it trough USB Type-C connector. We are using external chip for Type-C support but we are also need to distinguish between dedicated/host chargers. We found that USB-PHY supports BC standard. Does NXP USB stack support BC ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is USB_DEVICE_CHARGER_DETECT_ENABLE flag defined which suggests that such support is provided. After some digging in sources we also found that it needs FSL_FEATURE_SOC_USBDCD_COUNT set to compile. Unfortunately this flag is not defined in MIMXRT1051_features.h. Does that mean that RT1050 doesn't support BC or maybe USB stack is not yet prepared for BC support on RT1051 ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you shed some light on this issue ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Mateusz Piesta&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 08:52:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/RT105x-USB-BC-support/m-p/869376#M1495</guid>
      <dc:creator>mateuszpiesta</dc:creator>
      <dc:date>2019-01-29T08:52:13Z</dc:date>
    </item>
    <item>
      <title>Re: RT105x USB BC support</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/RT105x-USB-BC-support/m-p/869377#M1496</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mateusz Piesta&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;or maybe USB stack is not yet prepared for BC support on RT1051 ?&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;USBDCD is not in RT1050, this is why the FSL_FEATURE_SOC_USBDCD_COUNT is cero, in the RT1050 devices you can find the&amp;nbsp;USB_ANALOG in the USB-PHY part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This Phy is capable of the charger detection which &lt;EM&gt;"detects whether the upstream-facing device is connected to a down-stream facing charger, either a dedicated USB charger or a host charger". &lt;/EM&gt;Unfortunately, this is not implemented in the usb_phy.c file of the USB stack, so the customer would need to add it&lt;EM&gt;. &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 01:06:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/RT105x-USB-BC-support/m-p/869377#M1496</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2019-02-01T01:06:28Z</dc:date>
    </item>
  </channel>
</rss>