<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso General中的主题 i.MX6UL Flash Loader to Store SDK Example Program</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869363#M1490</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the I2C example in the MCUXpresso SDK.&amp;nbsp; It requires two NXP boards, a master and a slave, in order to demonstrate the communication.&amp;nbsp; Using IAR and an I-Jet debug pod, we can compile and run the "I2C Master" code on the master board, or the "I2C Slave" code on the slave board.&amp;nbsp; We only have one IDE license and debug probe, and cannot run the software on both boards using the debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the bare metal version of the SDK.&amp;nbsp; I cannot find any documentation that shows how to update the boot flash on the slave board so that it can run the I2C slave code upon boot-up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have found a flash loader binary file that appears to be compatible with our board.&amp;nbsp; It is located at the following path: IAR\EW 8.1\arm\config\flashloader\NXP\FlashIMX6UL_EVL_QSPI.out&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any documentation available that describes how to update the boot flash on the slave board?&amp;nbsp; If so, can someone please point me to this documentation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are the versions of the hardware and software that we are using:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Processor Kit:&amp;nbsp;&amp;nbsp; MCIMX6UL-EVKB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Base Board:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCIMX6UL-BB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Processor Board: MCIMX6UL-CM&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Processor:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCIMX6G2CVM05AA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Software&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;IDE: IAR Embedded Workbench 8.30.1&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Debug Probe: IAR I-jet&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;MCUXpresso Software Development Kit (SDK) Release Version: 2.2.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any help you can provide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dennis Jelcic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2019 01:17:00 GMT</pubDate>
    <dc:creator>dennis_jelcic</dc:creator>
    <dc:date>2019-01-11T01:17:00Z</dc:date>
    <item>
      <title>i.MX6UL Flash Loader to Store SDK Example Program</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869363#M1490</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the I2C example in the MCUXpresso SDK.&amp;nbsp; It requires two NXP boards, a master and a slave, in order to demonstrate the communication.&amp;nbsp; Using IAR and an I-Jet debug pod, we can compile and run the "I2C Master" code on the master board, or the "I2C Slave" code on the slave board.&amp;nbsp; We only have one IDE license and debug probe, and cannot run the software on both boards using the debugger.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using the bare metal version of the SDK.&amp;nbsp; I cannot find any documentation that shows how to update the boot flash on the slave board so that it can run the I2C slave code upon boot-up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have found a flash loader binary file that appears to be compatible with our board.&amp;nbsp; It is located at the following path: IAR\EW 8.1\arm\config\flashloader\NXP\FlashIMX6UL_EVL_QSPI.out&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any documentation available that describes how to update the boot flash on the slave board?&amp;nbsp; If so, can someone please point me to this documentation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are the versions of the hardware and software that we are using:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Processor Kit:&amp;nbsp;&amp;nbsp; MCIMX6UL-EVKB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Base Board:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCIMX6UL-BB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Processor Board: MCIMX6UL-CM&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Processor:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MCIMX6G2CVM05AA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Software&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;IDE: IAR Embedded Workbench 8.30.1&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Debug Probe: IAR I-jet&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;MCUXpresso Software Development Kit (SDK) Release Version: 2.2.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for any help you can provide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dennis Jelcic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 01:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869363#M1490</guid>
      <dc:creator>dennis_jelcic</dc:creator>
      <dc:date>2019-01-11T01:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL Flash Loader to Store SDK Example Program</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869364#M1491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;You could refer to section 5.2 “Using Manufacturing Tool” of the “Getting Started with MCUXpresso&lt;/P&gt;&lt;P&gt;SDK for i.MX 6UltraLite Derivatives” document regarding how to use MFGTool to download the example images (with some modifications) to Flash memory.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 15:21:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869364#M1491</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-01-15T15:21:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL Flash Loader to Store SDK Example Program</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869365#M1492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've looked on the NXP website, and on the internet, but I cannot find a document called “Getting Started with MCUXpresso SDK for i.MX 6UltraLite Derivatives”.&amp;nbsp; Could you please provide a link to the document, or a way for me to get a copy of it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Dennis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 23:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869365#M1492</guid>
      <dc:creator>dennis_jelcic</dc:creator>
      <dc:date>2019-01-15T23:44:32Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL Flash Loader to Store SDK Example Program</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869366#M1493</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dennis,&lt;/P&gt;&lt;P&gt;It is included on the documentation folder of the SDK installation path, like the following considering default paths:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;C:\nxp\SDK_2.2_MCIM6UL\docs&lt;/EM&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 15:47:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869366#M1493</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-01-16T15:47:17Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX6UL Flash Loader to Store SDK Example Program</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869367#M1494</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That was what we were looking for.&amp;nbsp; I was able to download an image to the QSPI Flash, and the board ran that program upon power-up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I had reviewed the document you mentioned previously, but had misunderstood the purpose of the MFGTool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dennis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 00:35:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/i-MX6UL-Flash-Loader-to-Store-SDK-Example-Program/m-p/869367#M1494</guid>
      <dc:creator>dennis_jelcic</dc:creator>
      <dc:date>2019-01-18T00:35:55Z</dc:date>
    </item>
  </channel>
</rss>