<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How do I debug without re-writing BOARD_FLASH? in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-debug-without-re-writing-BOARD-FLASH/m-p/861168#M1366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an application that uses around 50mb of flash storage on my iMXRT-1050EVKB. I want to debug certain parts of the application, but every time I want to test my code, it attempts to rewrite the ~50mb of data that should already be on the device. This process takes about 25-30 minutes, which is far too long to test minor changes. Is there a way to debug without rewriting the flash storage, as this never changes between builds?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Owen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Mar 2019 09:19:25 GMT</pubDate>
    <dc:creator>owen_phelan</dc:creator>
    <dc:date>2019-03-28T09:19:25Z</dc:date>
    <item>
      <title>How do I debug without re-writing BOARD_FLASH?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-debug-without-re-writing-BOARD-FLASH/m-p/861168#M1366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an application that uses around 50mb of flash storage on my iMXRT-1050EVKB. I want to debug certain parts of the application, but every time I want to test my code, it attempts to rewrite the ~50mb of data that should already be on the device. This process takes about 25-30 minutes, which is far too long to test minor changes. Is there a way to debug without rewriting the flash storage, as this never changes between builds?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Owen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 09:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-debug-without-re-writing-BOARD-FLASH/m-p/861168#M1366</guid>
      <dc:creator>owen_phelan</dc:creator>
      <dc:date>2019-03-28T09:19:25Z</dc:date>
    </item>
    <item>
      <title>Re: How do I debug without re-writing BOARD_FLASH?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-debug-without-re-writing-BOARD-FLASH/m-p/861169#M1367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Owen,&lt;/P&gt;&lt;P&gt;Yes, MCUXpresso can debug without program. Please select "verify only" in Debug Configurations.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64346i05205F974233070E/image-size/large?v=v2&amp;amp;px=999" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Mar 2019 07:18:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-debug-without-re-writing-BOARD-FLASH/m-p/861169#M1367</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-03-29T07:18:34Z</dc:date>
    </item>
  </channel>
</rss>