<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックDebug LPC54628 in command line using linkserver and gdb without GUI</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-LPC54628-in-command-line-using-linkserver-and-gdb-without/m-p/846003#M1166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Im working with LPC54628 on mcuexpresso debuging with linkserver and all works fine, but I wanna try debug it without&amp;nbsp; a gui. I meant start linkserver in command line and then connect to it from arm-none-eabi-gdb, but I don't know how. I need the configuration files needed by linkserver to connect to the uC properly, but I don't have it, and I can't see the precedure on the debug console in the GUI to copy that. My intention is to put that on a script and run it when I want to debug. Thanks in advance. Pablo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jan 2019 01:04:12 GMT</pubDate>
    <dc:creator>pablo_slavkin</dc:creator>
    <dc:date>2019-01-02T01:04:12Z</dc:date>
    <item>
      <title>Debug LPC54628 in command line using linkserver and gdb without GUI</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-LPC54628-in-command-line-using-linkserver-and-gdb-without/m-p/846003#M1166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Im working with LPC54628 on mcuexpresso debuging with linkserver and all works fine, but I wanna try debug it without&amp;nbsp; a gui. I meant start linkserver in command line and then connect to it from arm-none-eabi-gdb, but I don't know how. I need the configuration files needed by linkserver to connect to the uC properly, but I don't have it, and I can't see the precedure on the debug console in the GUI to copy that. My intention is to put that on a script and run it when I want to debug. Thanks in advance. Pablo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2019 01:04:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-LPC54628-in-command-line-using-linkserver-and-gdb-without/m-p/846003#M1166</guid>
      <dc:creator>pablo_slavkin</dc:creator>
      <dc:date>2019-01-02T01:04:12Z</dc:date>
    </item>
    <item>
      <title>Re: Debug LPC54628 in command line using linkserver and gdb without GUI</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debug-LPC54628-in-command-line-using-linkserver-and-gdb-without/m-p/846004#M1167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;A href="https://mcuxpresso.nxp.com/en/select"&gt;MCUXpresso SDK&lt;/A&gt; for LPC54628 support ARM GCC tool chain.&lt;/P&gt;&lt;P&gt;Please refer &amp;lt;&amp;lt;&lt;A href="https://www.nxp.com/docs/en/user-guide/MCUXSDKGSUG.pdf"&gt;Getting Started with MCUXpresso SDK&lt;/A&gt;&amp;gt;&amp;gt; document chapter 6 Run a demo using Arm GCC.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 05:30:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debug-LPC54628-in-command-line-using-linkserver-and-gdb-without/m-p/846004#M1167</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2019-01-07T05:30:19Z</dc:date>
    </item>
  </channel>
</rss>