<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックPINT GINT</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/PINT-GINT/m-p/841585#M1123</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing on the LPCXpresso 54102 development board using the SDK API ("fsl_" functions).&amp;nbsp; I noticed that the MCUXpresso SDK API Reference Manual includes two different interrupt drivers related to GPIO: GINT (see Chapter 12) and PINT (see Chapter 19).&amp;nbsp; I'm having trouble understanding why one would use one vs the other. Is there some difference in the underlying hardware which they address? PINT seems to be a bit more complex; does that mean GINT is deprecated, or are there situations where one might use both facilities in the same program?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Jul 2018 17:39:56 GMT</pubDate>
    <dc:creator>david_rick</dc:creator>
    <dc:date>2018-07-02T17:39:56Z</dc:date>
    <item>
      <title>PINT GINT</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/PINT-GINT/m-p/841585#M1123</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing on the LPCXpresso 54102 development board using the SDK API ("fsl_" functions).&amp;nbsp; I noticed that the MCUXpresso SDK API Reference Manual includes two different interrupt drivers related to GPIO: GINT (see Chapter 12) and PINT (see Chapter 19).&amp;nbsp; I'm having trouble understanding why one would use one vs the other. Is there some difference in the underlying hardware which they address? PINT seems to be a bit more complex; does that mean GINT is deprecated, or are there situations where one might use both facilities in the same program?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Jul 2018 17:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/PINT-GINT/m-p/841585#M1123</guid>
      <dc:creator>david_rick</dc:creator>
      <dc:date>2018-07-02T17:39:56Z</dc:date>
    </item>
    <item>
      <title>Re: PINT GINT</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/PINT-GINT/m-p/841586#M1124</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David Rick,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;From the general function perspective, the GINT and PINT module are similar.&lt;BR /&gt;Definitely, they're not same, the GINT is capable of enabling interrupts through an OR or AND operation, so it's suited for a combined group of pins, however, PINT is suited for a particular pin.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jul 2018 02:25:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/PINT-GINT/m-p/841586#M1124</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-07-04T02:25:06Z</dc:date>
    </item>
  </channel>
</rss>