<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem using cache in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Problem-using-cache/m-p/837141#M1091</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using MCUXpresso 10.2.1 with a custom board based on MK66FN2M0.&lt;/P&gt;&lt;P&gt;I developed an application that is working fine, but on&amp;nbsp;some operations it's a little&amp;nbsp;time consuming. I've enabled the cache memory with LMEM module, but I haven't seen any speed gain.&lt;/P&gt;&lt;P&gt;I've used the following statement:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LMEM_EnableCodeCache( LMEM, true );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do some other configurations are needed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Biafra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Oct 2018 13:43:53 GMT</pubDate>
    <dc:creator>biafra</dc:creator>
    <dc:date>2018-10-25T13:43:53Z</dc:date>
    <item>
      <title>Problem using cache</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problem-using-cache/m-p/837141#M1091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using MCUXpresso 10.2.1 with a custom board based on MK66FN2M0.&lt;/P&gt;&lt;P&gt;I developed an application that is working fine, but on&amp;nbsp;some operations it's a little&amp;nbsp;time consuming. I've enabled the cache memory with LMEM module, but I haven't seen any speed gain.&lt;/P&gt;&lt;P&gt;I've used the following statement:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LMEM_EnableCodeCache( LMEM, true );&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do some other configurations are needed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Biafra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2018 13:43:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problem-using-cache/m-p/837141#M1091</guid>
      <dc:creator>biafra</dc:creator>
      <dc:date>2018-10-25T13:43:53Z</dc:date>
    </item>
    <item>
      <title>Re: Problem using cache</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problem-using-cache/m-p/837142#M1092</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Biafra,&lt;/P&gt;&lt;P&gt;This function is enough to enable 8k I/D cache. Cache will not dramatically increase the speed. But it really work. I spent some time to test by Coremark. The total ticks drop from 1727 to 1574 after I enable cache.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Oct 2018 08:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problem-using-cache/m-p/837142#M1092</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-10-26T08:41:57Z</dc:date>
    </item>
  </channel>
</rss>