<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: Boot from SD using MFGTools + MCUXpresso + RT1050EVK</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835162#M1059</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alice,&lt;/P&gt;&lt;P&gt;How to generate boot_image.sb file from s19 for MIMXRT1050-EVK board, to boot from SD card.&lt;/P&gt;&lt;P&gt;Need to know .bd file modification, MCUXpresso IDE memory configuration and elftosb?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 19 Jan 2019 06:12:19 GMT</pubDate>
    <dc:creator>chum</dc:creator>
    <dc:date>2019-01-19T06:12:19Z</dc:date>
    <item>
      <title>Boot from SD using MFGTools + MCUXpresso + RT1050EVK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835159#M1056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did anyone try to program boot image created under MCUXpresso into SDCard ? My goal is to boot from eMMC but as first step I would like to boot from sdcard and later switch to eMMC. I successfuly managed to create boot_image.sb file and I am able to program it into SDCard but after reconfiguring boot pins and reset program won't boot. I am following steps described in AN12107 but unfortunately project configure related steps are for IAR.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My configuration:&lt;/P&gt;&lt;P&gt;- application code executed from DTCM&lt;/P&gt;&lt;P&gt;- I modified linker script to put reset vector and rest of the app code under 0x20002000 address&lt;/P&gt;&lt;P&gt;- in "imx-dtcm-unsigned.bm" file i set startAddress = 0x20000000 and&amp;nbsp;entryPointAddress = 0x20002000 (that's where vectors are)&lt;/P&gt;&lt;P&gt;- I am using "program_sdcard_image.bd" without any custom changes&lt;/P&gt;&lt;P&gt;- I'm using hello_blinky example project as base&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;EDIT: After some reading and searching I believe entryPointAddress&amp;nbsp;should be set to&amp;nbsp;0x20002000&amp;nbsp;(vectors array start address). Still I don't know if I should set&amp;nbsp;startAddress&amp;nbsp;to&amp;nbsp;0x20000000&amp;nbsp; or to different address ? I also recreated example SD card boot example from AN12107(section 3.5) using ITCM but I'm facing the same problem, app won't boot. Why is it necessary to set&amp;nbsp;startAddress&lt;SPAN&gt;&amp;nbsp;to 0x8000 ? Why it can't be beginning of ITCM memory ?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I would be grateful for any info, example or simple tutorial.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks in advance&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Mateusz Piesta&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 07:57:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835159#M1056</guid>
      <dc:creator>mateuszpiesta</dc:creator>
      <dc:date>2018-07-20T07:57:43Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SD using MFGTools + MCUXpresso + RT1050EVK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835160#M1057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN&gt;Mateusz Piesta,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please change startAddress from 0x8000 to 0x1000 to have a try on with TICM proejct. . &lt;A href="https://community.nxp.com/message/997860"&gt;https://community.nxp.com/message/997860&lt;/A&gt;&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If still can't work, please tell me the version of SDK , and MCUXpresso IDE.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Alice&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 07:13:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835160#M1057</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-07-24T07:13:46Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SD using MFGTools + MCUXpresso + RT1050EVK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835161#M1058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN&gt;Mateusz Piesta&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;I test it on my side today , it can work well.&lt;/P&gt;&lt;P&gt;MCUXpresso IDE v10.2.0_759&lt;/P&gt;&lt;P&gt;SDK v2.4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the SDK demo of "hello_world"， only change memory configuration:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66420i2C18A0956ED968E1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please pay attention the start address of application is 0x2000,.&lt;/P&gt;&lt;P&gt;Then refer to AN12107 steps to do .&lt;/P&gt;&lt;P&gt;If have any problem about this, you can share it with us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 09:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835161#M1058</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-07-25T09:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SD using MFGTools + MCUXpresso + RT1050EVK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835162#M1059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alice,&lt;/P&gt;&lt;P&gt;How to generate boot_image.sb file from s19 for MIMXRT1050-EVK board, to boot from SD card.&lt;/P&gt;&lt;P&gt;Need to know .bd file modification, MCUXpresso IDE memory configuration and elftosb?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Jan 2019 06:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835162#M1059</guid>
      <dc:creator>chum</dc:creator>
      <dc:date>2019-01-19T06:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from SD using MFGTools + MCUXpresso + RT1050EVK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835163#M1060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just finished a deatailed tutorial on that subject:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2019/01/22/tutorial-booting-the-nxp-i-mx-rt-from-micro-sd-card/" title="https://mcuoneclipse.com/2019/01/22/tutorial-booting-the-nxp-i-mx-rt-from-micro-sd-card/"&gt;Tutorial: Booting the NXP i.MX RT from Micro SD Card | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2019 21:56:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Boot-from-SD-using-MFGTools-MCUXpresso-RT1050EVK/m-p/835163#M1060</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2019-01-22T21:56:58Z</dc:date>
    </item>
  </channel>
</rss>