<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCUXpresso Config Tools seems to generate a 'wrong' SDK in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-Config-Tools-seems-to-generate-a-wrong-SDK/m-p/608428#M10</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;(chip I use: MKL02Z32)&lt;/P&gt;&lt;P&gt;- The pin tool has a wrong mux config (Alt2, I2C0_{SCL/SDA} on C3/D4 mixed up)&lt;/P&gt;&lt;P&gt;- device driver for adc16 but not adc12,&amp;nbsp;FSL_FEATURE_SOC_ADC16_COUNT is set to 1 (no 16bit adc on this chip)&lt;/P&gt;&lt;P&gt;- no uart driver, no uart according x_features.h, but chip has a low power uart&lt;/P&gt;&lt;P&gt;- probably more...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Feb 2017 13:36:34 GMT</pubDate>
    <dc:creator>gartin</dc:creator>
    <dc:date>2017-02-28T13:36:34Z</dc:date>
    <item>
      <title>MCUXpresso Config Tools seems to generate a 'wrong' SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-Config-Tools-seems-to-generate-a-wrong-SDK/m-p/608428#M10</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;(chip I use: MKL02Z32)&lt;/P&gt;&lt;P&gt;- The pin tool has a wrong mux config (Alt2, I2C0_{SCL/SDA} on C3/D4 mixed up)&lt;/P&gt;&lt;P&gt;- device driver for adc16 but not adc12,&amp;nbsp;FSL_FEATURE_SOC_ADC16_COUNT is set to 1 (no 16bit adc on this chip)&lt;/P&gt;&lt;P&gt;- no uart driver, no uart according x_features.h, but chip has a low power uart&lt;/P&gt;&lt;P&gt;- probably more...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 13:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-Config-Tools-seems-to-generate-a-wrong-SDK/m-p/608428#M10</guid>
      <dc:creator>gartin</dc:creator>
      <dc:date>2017-02-28T13:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Config Tools seems to generate a 'wrong' SDK</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-Config-Tools-seems-to-generate-a-wrong-SDK/m-p/608429#M11</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Martin,&lt;/P&gt;&lt;P&gt;Thank you for reporting issues. We have fixed the first issue of the incorrect pin muxing of SCL/SDA. The fixed version of the data will be available in the next release.&lt;/P&gt;&lt;P&gt;The MKL02Z32 derivative have the SAR ADC16 device that is limited to 12bits resolution only (MCU specific). Therefore the fsl_adc16 driver is compatible to this device and it is available for the MKL02Z32.&lt;/P&gt;&lt;P&gt;The UART device (available on the MKL02Z32) is supported by the fsl_lpsci driver in the SDK 2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Mar 2017 15:33:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-Config-Tools-seems-to-generate-a-wrong-SDK/m-p/608429#M11</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2017-03-20T15:33:50Z</dc:date>
    </item>
  </channel>
</rss>