<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Secure Provision Tool 25.12 failed to run after installation in MCUXpresso Secure Provisioning Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provision-Tool-25-12-failed-to-run-after-installation/m-p/2332226#M718</link>
    <description>&lt;P&gt;Following is the log :Traceback (most recent call last):&lt;BR /&gt;File "pyi_rth_pkgres.py", line 177, in &amp;lt;module&amp;gt;&lt;BR /&gt;File "pyi_rth_pkgres.py", line 44, in _pyi_rthook&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 1360, in _find_and_load&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 1331, in _find_and_load_unlocked&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 935, in _load_unlocked&lt;BR /&gt;File "pyimod02_importers.py", line 457, in exec_module&lt;BR /&gt;File "pkg_resources\__init__.py", line 90, in &amp;lt;module&amp;gt;&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 1360, in _find_and_load&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 1331, in _find_and_load_unlocked&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 935, in _load_unlocked&lt;BR /&gt;File "pyimod02_importers.py", line 457, in exec_module&lt;BR /&gt;File "setuptools\_vendor\jaraco\text\__init__.py", line 231, in &amp;lt;module&amp;gt;&lt;BR /&gt;File "pathlib.py", line 1028, in read_text&lt;BR /&gt;File "&amp;lt;frozen codecs&amp;gt;", line 322, in decode&lt;BR /&gt;UnicodeDecodeError: 'utf-8' codec can't decode byte 0xee in position 6: invalid continuation byte&lt;BR /&gt;[PYI-30324:ERROR] Failed to execute script 'pyi_rth_pkgres' due to unhandled exception!&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;What caused it?&lt;/P&gt;</description>
    <pubDate>Fri, 13 Mar 2026 06:47:17 GMT</pubDate>
    <dc:creator>nxf51434</dc:creator>
    <dc:date>2026-03-13T06:47:17Z</dc:date>
    <item>
      <title>Secure Provision Tool 25.12 failed to run after installation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provision-Tool-25-12-failed-to-run-after-installation/m-p/2332226#M718</link>
      <description>&lt;P&gt;Following is the log :Traceback (most recent call last):&lt;BR /&gt;File "pyi_rth_pkgres.py", line 177, in &amp;lt;module&amp;gt;&lt;BR /&gt;File "pyi_rth_pkgres.py", line 44, in _pyi_rthook&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 1360, in _find_and_load&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 1331, in _find_and_load_unlocked&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 935, in _load_unlocked&lt;BR /&gt;File "pyimod02_importers.py", line 457, in exec_module&lt;BR /&gt;File "pkg_resources\__init__.py", line 90, in &amp;lt;module&amp;gt;&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 1360, in _find_and_load&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 1331, in _find_and_load_unlocked&lt;BR /&gt;File "&amp;lt;frozen importlib._bootstrap&amp;gt;", line 935, in _load_unlocked&lt;BR /&gt;File "pyimod02_importers.py", line 457, in exec_module&lt;BR /&gt;File "setuptools\_vendor\jaraco\text\__init__.py", line 231, in &amp;lt;module&amp;gt;&lt;BR /&gt;File "pathlib.py", line 1028, in read_text&lt;BR /&gt;File "&amp;lt;frozen codecs&amp;gt;", line 322, in decode&lt;BR /&gt;UnicodeDecodeError: 'utf-8' codec can't decode byte 0xee in position 6: invalid continuation byte&lt;BR /&gt;[PYI-30324:ERROR] Failed to execute script 'pyi_rth_pkgres' due to unhandled exception!&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;What caused it?&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 06:47:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provision-Tool-25-12-failed-to-run-after-installation/m-p/2332226#M718</guid>
      <dc:creator>nxf51434</dc:creator>
      <dc:date>2026-03-13T06:47:17Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Provision Tool 25.12 failed to run after installation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provision-Tool-25-12-failed-to-run-after-installation/m-p/2332254#M719</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;can you check if the following file was installed and can you attach the file to the chat?&lt;/P&gt;
&lt;P&gt;"c:\nxp\SEC_Provi_25.12\bin\_internal\setuptools\_vendor\jaraco\text\Lorem ipsum.txt"&lt;/P&gt;
&lt;P&gt;Based on the stack trace it seems the file is broken.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you confirm you are running the tool on Windows 11?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Can you provide info about language and region configuration of your OS (Start &amp;gt; Settings &amp;gt; Time &amp;amp; language &amp;gt; Language &amp;amp; region)?&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 07:39:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provision-Tool-25-12-failed-to-run-after-installation/m-p/2332254#M719</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2026-03-13T07:39:40Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Provision Tool 25.12 failed to run after installation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provision-Tool-25-12-failed-to-run-after-installation/m-p/2332266#M720</link>
      <description>&lt;P&gt;Based on your indication, the issue caused by the encryption software installed on the local computer. After adding the application to the whitelist, the problem was resolved.&lt;/P&gt;</description>
      <pubDate>Fri, 13 Mar 2026 07:57:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provision-Tool-25-12-failed-to-run-after-installation/m-p/2332266#M720</guid>
      <dc:creator>nxf51434</dc:creator>
      <dc:date>2026-03-13T07:57:47Z</dc:date>
    </item>
  </channel>
</rss>