<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic BEE USER KEYS boot+app in MCUXpresso Secure Provisioning Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/BEE-USER-KEYS-boot-app/m-p/2009452#M521</link>
    <description>&lt;P&gt;hi:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I refactored app.bin with the command and generated app-2.bin. After burning it in, the code couldn't run. I don't know where the problem lies?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="acallamp_0-1733545628336.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314650i495714E107366A34/image-size/medium?v=v2&amp;amp;px=400" role="button" title="acallamp_0-1733545628336.png" alt="acallamp_0-1733545628336.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="acallamp_1-1733545663027.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314651i9E5EAC626B5A8569/image-size/medium?v=v2&amp;amp;px=400" role="button" title="acallamp_1-1733545663027.png" alt="acallamp_1-1733545663027.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;# =========== BEE configuration ===========&lt;BR /&gt;# ----------------------------------------------------------------------------------------------------&lt;BR /&gt;# == Basic Settings ==&lt;BR /&gt;# ----------------------------------------------------------------------------------------------------&lt;BR /&gt;output_folder: "../bootable_images" # [Required], BEE output folder; Folder name to store generated BEE output&lt;BR /&gt;input_binary: "../bootable_images/boot_hab.bin" # [Required], Input binary file; Path to input binary file&lt;BR /&gt;output_name: "../bootable_images/Position.bin" # [Optional], Output binary file name; File name of the encrypted file, output_folder/output_name&lt;BR /&gt;header_name: "bee_ehdr" # [Optional], File name of the exported BEE region headers; output_folder/header_name + index will be prepended&lt;/P&gt;&lt;P&gt;output_folder: "../bootable_images" # [Required], BEE output folder; Folder name to store generated BEE output&lt;BR /&gt;input_binary: "../bootable_images/app.bin" # [Required], Input binary file; Path to input binary file&lt;BR /&gt;output_name: "../bootable_images/app-2.bin" # [Optional], Output binary file name; File name of the encrypted file, output_folder/output_name&lt;BR /&gt;# ----------------------------------------------------------------------------------------------------&lt;BR /&gt;# == BEE Settings ==&lt;BR /&gt;# ----------------------------------------------------------------------------------------------------&lt;BR /&gt;engine_selection: engine0 # [Required], Engine selection; BEE Engine Selection, engine0, engine1 or both engines; Possible options:['engine0', 'engine1', 'both']&lt;BR /&gt;engine_key_selection: zero # [Required], Engine Key selection; Random Key or Zero key; Possible options:['random', 'zero']&lt;BR /&gt;base_address: '0x60001000' # [Required], Base address of the image&lt;BR /&gt;bee_engine: # [Required], Bee engines; Configuration of BEE engines&lt;BR /&gt;# # # Engine 0 # # #&lt;BR /&gt;- bee_cfg: # [Required], Engine Config; BEE engine configuration&lt;BR /&gt;user_key: 0x64847E37868D2391B95A6D54DAB19DC2 # [Required], User AES-128 key; AES key for encryption&lt;BR /&gt;protected_region: # [Optional], Protected region; List of protected regions, up to four regions&lt;BR /&gt;- start_address: '0x60001000' # [Required], Start address of protected region, it should be aligned to 1 KB (1024 B)&lt;BR /&gt;length: '0x0000A800' # [Required], Length of protected region, it should be aligned to 1 KB (1024 B)&lt;BR /&gt;protected_level: 0 # [Required], Protected level (0/1/2/3), 0 is default&lt;BR /&gt;- start_address: '0x60020000' # [Required], Start address of protected region, it should be aligned to 1 KB (1024 B)&lt;BR /&gt;length: '0x0000B800' # [Required], Length of protected region, it should be aligned to 1 KB (1024 B)&lt;BR /&gt;protected_level: 0 # [Required], Protected level (0/1/2/3), 0 is default&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 07 Dec 2024 04:32:30 GMT</pubDate>
    <dc:creator>acallamp</dc:creator>
    <dc:date>2024-12-07T04:32:30Z</dc:date>
    <item>
      <title>BEE USER KEYS boot+app</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/BEE-USER-KEYS-boot-app/m-p/2009452#M521</link>
      <description>&lt;P&gt;hi:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I refactored app.bin with the command and generated app-2.bin. After burning it in, the code couldn't run. I don't know where the problem lies?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="acallamp_0-1733545628336.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314650i495714E107366A34/image-size/medium?v=v2&amp;amp;px=400" role="button" title="acallamp_0-1733545628336.png" alt="acallamp_0-1733545628336.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="acallamp_1-1733545663027.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314651i9E5EAC626B5A8569/image-size/medium?v=v2&amp;amp;px=400" role="button" title="acallamp_1-1733545663027.png" alt="acallamp_1-1733545663027.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;# =========== BEE configuration ===========&lt;BR /&gt;# ----------------------------------------------------------------------------------------------------&lt;BR /&gt;# == Basic Settings ==&lt;BR /&gt;# ----------------------------------------------------------------------------------------------------&lt;BR /&gt;output_folder: "../bootable_images" # [Required], BEE output folder; Folder name to store generated BEE output&lt;BR /&gt;input_binary: "../bootable_images/boot_hab.bin" # [Required], Input binary file; Path to input binary file&lt;BR /&gt;output_name: "../bootable_images/Position.bin" # [Optional], Output binary file name; File name of the encrypted file, output_folder/output_name&lt;BR /&gt;header_name: "bee_ehdr" # [Optional], File name of the exported BEE region headers; output_folder/header_name + index will be prepended&lt;/P&gt;&lt;P&gt;output_folder: "../bootable_images" # [Required], BEE output folder; Folder name to store generated BEE output&lt;BR /&gt;input_binary: "../bootable_images/app.bin" # [Required], Input binary file; Path to input binary file&lt;BR /&gt;output_name: "../bootable_images/app-2.bin" # [Optional], Output binary file name; File name of the encrypted file, output_folder/output_name&lt;BR /&gt;# ----------------------------------------------------------------------------------------------------&lt;BR /&gt;# == BEE Settings ==&lt;BR /&gt;# ----------------------------------------------------------------------------------------------------&lt;BR /&gt;engine_selection: engine0 # [Required], Engine selection; BEE Engine Selection, engine0, engine1 or both engines; Possible options:['engine0', 'engine1', 'both']&lt;BR /&gt;engine_key_selection: zero # [Required], Engine Key selection; Random Key or Zero key; Possible options:['random', 'zero']&lt;BR /&gt;base_address: '0x60001000' # [Required], Base address of the image&lt;BR /&gt;bee_engine: # [Required], Bee engines; Configuration of BEE engines&lt;BR /&gt;# # # Engine 0 # # #&lt;BR /&gt;- bee_cfg: # [Required], Engine Config; BEE engine configuration&lt;BR /&gt;user_key: 0x64847E37868D2391B95A6D54DAB19DC2 # [Required], User AES-128 key; AES key for encryption&lt;BR /&gt;protected_region: # [Optional], Protected region; List of protected regions, up to four regions&lt;BR /&gt;- start_address: '0x60001000' # [Required], Start address of protected region, it should be aligned to 1 KB (1024 B)&lt;BR /&gt;length: '0x0000A800' # [Required], Length of protected region, it should be aligned to 1 KB (1024 B)&lt;BR /&gt;protected_level: 0 # [Required], Protected level (0/1/2/3), 0 is default&lt;BR /&gt;- start_address: '0x60020000' # [Required], Start address of protected region, it should be aligned to 1 KB (1024 B)&lt;BR /&gt;length: '0x0000B800' # [Required], Length of protected region, it should be aligned to 1 KB (1024 B)&lt;BR /&gt;protected_level: 0 # [Required], Protected level (0/1/2/3), 0 is default&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 07 Dec 2024 04:32:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/BEE-USER-KEYS-boot-app/m-p/2009452#M521</guid>
      <dc:creator>acallamp</dc:creator>
      <dc:date>2024-12-07T04:32:30Z</dc:date>
    </item>
    <item>
      <title>Re: BEE USER KEYS boot+app</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/BEE-USER-KEYS-boot-app/m-p/2010312#M524</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;it is not clear what you have exactly did. If you put all into one bee_config.yaml file, then it won't work, because you cannot have multiple input_binary, output_name attributes, only one will be used. It is not an array.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;May be either:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;first encrypt app.bin as it is main application (Source input image on Build tab) and after encryption use it as an additional image,&lt;/LI&gt;
&lt;LI&gt;or create a separate BEE YAML&amp;nbsp; file just for app.bin and create manually in a command line.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Dec 2024 16:09:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/BEE-USER-KEYS-boot-app/m-p/2010312#M524</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2024-12-09T16:09:23Z</dc:date>
    </item>
  </channel>
</rss>