<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1052  Start FlashLoader error in MCUXpresso Secure Provisioning Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005911#M510</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;for flashloader I'd ask for help in one of the these forums&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/MCU-Bootloader/bd-p/MCUBOOT" target="_blank"&gt;https://community.nxp.com/t5/MCU-Bootloader/bd-p/MCUBOOT&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;or here &lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/bd-p/mcuxpresso-sdk" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-SDK/bd-p/mcuxpresso-sdk&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
    <pubDate>Tue, 03 Dec 2024 09:24:28 GMT</pubDate>
    <dc:creator>liborukropec</dc:creator>
    <dc:date>2024-12-03T09:24:28Z</dc:date>
    <item>
      <title>RT1052  Start FlashLoader error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005557#M507</link>
      <description>&lt;P&gt;### Start FlashLoader ###&lt;BR /&gt;sdphost -p COM9,115200 -j -- jump-address 0x20001C00&lt;BR /&gt;Status (HAB mode) = 1450735702 (0x56787856) Hab Is Disabled (Unlocked).&lt;BR /&gt;sdphost succeeded, HAB disabled&lt;BR /&gt;### Waiting FlashLoader to be initialized for 10 seconds ###&lt;BR /&gt;### Timeout wait value can be adjusted from Preferences ###&lt;BR /&gt;### Check presence of FlashLoader ###&lt;BR /&gt;blhost -t 2000 -p COM9,115200 -j -- get-property 1 0&lt;BR /&gt;SpsdkNoDeviceFoundError: No devices for given interface 'uart' and parameters 'port=COM9, baudrate=115200, timeout=2000' was found.&lt;BR /&gt;blhost failed&lt;/P&gt;&lt;P&gt;HI:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;I can run it successfully on the development board, but I cannot run it on the product board. The hardware difference is that the product board does not have an RTC crystal oscillator. Do I need to use RTC to run FlashLoader?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Dec 2024 01:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005557#M507</guid>
      <dc:creator>acallamp</dc:creator>
      <dc:date>2024-12-03T01:45:41Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052  Start FlashLoader error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005768#M508</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;flashloader is a MCUXpresso SDK apllication. You can download the SDK from &lt;A href="https://mcuxpresso.nxp.com" target="_blank" rel="noopener"&gt;https://mcuxpresso.nxp.com,&lt;/A&gt; see example project named "flashloader" and try to debug on your production board. You can customize it and replace the binary flashloader image distributed in MCUXpresso Secure Provisioning tool with your custom version.&lt;/P&gt;
&lt;P&gt;About the requirements for the flashloader application, kindly refer to the description of the MCUXpresso SDK project.&lt;/P&gt;</description>
      <pubDate>Tue, 03 Dec 2024 07:12:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005768#M508</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2024-12-03T07:12:28Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052  Start FlashLoader error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005797#M509</link>
      <description>HI：&lt;BR /&gt;Expert, I tried your method and ran it with SDK. The result is still the same. The development board is good, but the product board is not, and the simulation is not very stable. The code is quite large and the manual is not clear. For a while, I didn't know where to look for the reason. Is it a hardware issue? Or is it a software issue? Can you give some tips on where to start? thank you</description>
      <pubDate>Tue, 03 Dec 2024 07:46:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005797#M509</guid>
      <dc:creator>acallamp</dc:creator>
      <dc:date>2024-12-03T07:46:07Z</dc:date>
    </item>
    <item>
      <title>Re: RT1052  Start FlashLoader error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005911#M510</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;for flashloader I'd ask for help in one of the these forums&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://community.nxp.com/t5/MCU-Bootloader/bd-p/MCUBOOT" target="_blank"&gt;https://community.nxp.com/t5/MCU-Bootloader/bd-p/MCUBOOT&lt;/A&gt;&lt;/LI&gt;
&lt;LI&gt;or here &lt;A href="https://community.nxp.com/t5/MCUXpresso-SDK/bd-p/mcuxpresso-sdk" target="_blank"&gt;https://community.nxp.com/t5/MCUXpresso-SDK/bd-p/mcuxpresso-sdk&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
      <pubDate>Tue, 03 Dec 2024 09:24:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/RT1052-Start-FlashLoader-error/m-p/2005911#M510</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2024-12-03T09:24:28Z</dc:date>
    </item>
  </channel>
</rss>