<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Secure Provisioning ToolのトピックIMXRT1052 XIP Encryption Issue</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/IMXRT1052-XIP-Encryption-Issue/m-p/2004673#M504</link>
    <description>&lt;P&gt;&lt;SPAN&gt;May I ask the expert: RT1052+XIP encryption method? If I want to use the UID of the chip as the key without burning the fuse, which solution should I choose to encrypt and generate the image? Because I am worried that after burning the fuse, the chip cannot be reused. May I ask if there are any good methods for encryption. It is also beneficial for the factory to facilitate mass production.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 02 Dec 2024 02:14:37 GMT</pubDate>
    <dc:creator>acallamp</dc:creator>
    <dc:date>2024-12-02T02:14:37Z</dc:date>
    <item>
      <title>IMXRT1052 XIP Encryption Issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/IMXRT1052-XIP-Encryption-Issue/m-p/2004673#M504</link>
      <description>&lt;P&gt;&lt;SPAN&gt;May I ask the expert: RT1052+XIP encryption method? If I want to use the UID of the chip as the key without burning the fuse, which solution should I choose to encrypt and generate the image? Because I am worried that after burning the fuse, the chip cannot be reused. May I ask if there are any good methods for encryption. It is also beneficial for the factory to facilitate mass production.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 02:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/IMXRT1052-XIP-Encryption-Issue/m-p/2004673#M504</guid>
      <dc:creator>acallamp</dc:creator>
      <dc:date>2024-12-02T02:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1052 XIP Encryption Issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/IMXRT1052-XIP-Encryption-Issue/m-p/2004850#M505</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;"Encrypted mode with UID" =&amp;gt; "BEE with OTPMK". The mode is available only for signed images, so it will require to burn fuses for signing.&lt;/P&gt;
&lt;P&gt;You can always review, which fuses will be burnt in:&lt;/P&gt;
&lt;P&gt;1) OTP Configuration dialog (use filter "Required")&lt;/P&gt;
&lt;P&gt;2) Prior the write script is executed, the GUI tool first check the fuses in the processor and then displays all irreversible changes.&lt;/P&gt;
&lt;P&gt;After the fuses burnt, the chip still can be used with the same keys. Fuse bit burnt to 1 cannot be reverted to 0 anymore.&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;gt; May I ask if there are any good methods for encryption&lt;/EM&gt;&lt;BR /&gt;You need to decide, whether you need same flash content for all products. If yes, you need same key for all products and you must use user key. Using UID/OTPMK means each product uses different key, so flash content is different. &lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 02 Dec 2024 06:54:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/IMXRT1052-XIP-Encryption-Issue/m-p/2004850#M505</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2024-12-02T06:54:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMXRT1052 XIP Encryption Issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/IMXRT1052-XIP-Encryption-Issue/m-p/2004904#M506</link>
      <description>HI：&lt;BR /&gt;Does MFGTOOL only support USB and have production software that supports UART？</description>
      <pubDate>Mon, 02 Dec 2024 07:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/IMXRT1052-XIP-Encryption-Issue/m-p/2004904#M506</guid>
      <dc:creator>acallamp</dc:creator>
      <dc:date>2024-12-02T07:41:26Z</dc:date>
    </item>
  </channel>
</rss>