<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic nxpimage: how to accept input file on command line instead of config entry in MCUXpresso Secure Provisioning Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/nxpimage-how-to-accept-input-file-on-command-line-instead-of/m-p/1977015#M425</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;.bd file has the following entry:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;sources {
    elfFile = extern(0);
}&lt;/LI-CODE&gt;&lt;P&gt;doing this nxpimage expects the name of the input file on the command line.&lt;BR /&gt;How can I achieve the same behavior using .yaml files?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;</description>
    <pubDate>Fri, 18 Oct 2024 10:23:45 GMT</pubDate>
    <dc:creator>mastupristi</dc:creator>
    <dc:date>2024-10-18T10:23:45Z</dc:date>
    <item>
      <title>nxpimage: how to accept input file on command line instead of config entry</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/nxpimage-how-to-accept-input-file-on-command-line-instead-of/m-p/1977015#M425</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;.bd file has the following entry:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;sources {
    elfFile = extern(0);
}&lt;/LI-CODE&gt;&lt;P&gt;doing this nxpimage expects the name of the input file on the command line.&lt;BR /&gt;How can I achieve the same behavior using .yaml files?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;</description>
      <pubDate>Fri, 18 Oct 2024 10:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/nxpimage-how-to-accept-input-file-on-command-line-instead-of/m-p/1977015#M425</guid>
      <dc:creator>mastupristi</dc:creator>
      <dc:date>2024-10-18T10:23:45Z</dc:date>
    </item>
    <item>
      <title>Re: nxpimage: how to accept input file on command line instead of config entry</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/nxpimage-how-to-accept-input-file-on-command-line-instead-of/m-p/1978216#M429</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/124967"&gt;@mastupristi&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;The nxpimage -&amp;gt; hab application supports both bd files and YAML configuration files. The bd file support is primarily intended as a backward compatibility solution for customers transitioning from elftosb to spsdk. I recommend using YAML configurations, as this is the standard format across all spsdk applications.&lt;/P&gt;
&lt;P&gt;Unfortunately, passing the input image via the command line when using YAML configuration is not currently supported.&lt;/P&gt;
&lt;P&gt;However, we are exploring the possibility of allowing users to override any configuration parameter across all spsdk applications. If implemented, this would enable you to specify the elfFile as a command line parameter when using a YAML file. Please note that this feature has not yet been developed.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me know if you need any further adjustments!&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 11:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/nxpimage-how-to-accept-input-file-on-command-line-instead-of/m-p/1978216#M429</guid>
      <dc:creator>nxf93270</dc:creator>
      <dc:date>2024-10-21T11:48:37Z</dc:date>
    </item>
  </channel>
</rss>