<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SEC Tool v7 write image script points to improper installation bin for different scripts. in MCUXpresso Secure Provisioning Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1758581#M307</link>
    <description>&lt;P&gt;We identified a potential bug with the generation of write_image scripts for SEC tool v7.&lt;/P&gt;&lt;P&gt;The installation directory for SEC Tool v7 varies on host computer. For Windows, it is:&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;export&lt;/SPAN&gt; &lt;SPAN&gt;"SPT_INSTALL_BIN=C:/nxp/MCUX_Provi_v7/bin"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;For Mac/Linux, it is:&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;export&lt;/SPAN&gt; &lt;SPAN&gt;"SPT_INSTALL_BIN=/opt/nxp/MCUX_Provi_v7/bin"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;When using SEC Tool v7 on Linux, all install bin directories point to&amp;nbsp;opt/nxp/MCUX_Provi_v7/bin regardless of if the write_image is a windows batch script file. The same holds true when using the SEC Tool v7 on a Windows machine, but instead to&amp;nbsp;C:/nxp/MCUX_Provi_v7/bin for the .sh scripts&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Because of the differences in installation directory, creating a manufacturing package is not cross-compatible unless the specified line in the&amp;nbsp; write script is changed to point to the appropriate installation directory for the host OS. We're hoping this gets addressed in the next version update so that our team can generate manufacturing packages independent of host operating system.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Thu, 16 Nov 2023 19:50:33 GMT</pubDate>
    <dc:creator>george_iyo</dc:creator>
    <dc:date>2023-11-16T19:50:33Z</dc:date>
    <item>
      <title>SEC Tool v7 write image script points to improper installation bin for different scripts.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1758581#M307</link>
      <description>&lt;P&gt;We identified a potential bug with the generation of write_image scripts for SEC tool v7.&lt;/P&gt;&lt;P&gt;The installation directory for SEC Tool v7 varies on host computer. For Windows, it is:&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;export&lt;/SPAN&gt; &lt;SPAN&gt;"SPT_INSTALL_BIN=C:/nxp/MCUX_Provi_v7/bin"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;For Mac/Linux, it is:&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;export&lt;/SPAN&gt; &lt;SPAN&gt;"SPT_INSTALL_BIN=/opt/nxp/MCUX_Provi_v7/bin"&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;When using SEC Tool v7 on Linux, all install bin directories point to&amp;nbsp;opt/nxp/MCUX_Provi_v7/bin regardless of if the write_image is a windows batch script file. The same holds true when using the SEC Tool v7 on a Windows machine, but instead to&amp;nbsp;C:/nxp/MCUX_Provi_v7/bin for the .sh scripts&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Because of the differences in installation directory, creating a manufacturing package is not cross-compatible unless the specified line in the&amp;nbsp; write script is changed to point to the appropriate installation directory for the host OS. We're hoping this gets addressed in the next version update so that our team can generate manufacturing packages independent of host operating system.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 16 Nov 2023 19:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1758581#M307</guid>
      <dc:creator>george_iyo</dc:creator>
      <dc:date>2023-11-16T19:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: SEC Tool v7 write image script points to improper installation bin for different scripts.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1759629#M308</link>
      <description>&lt;P&gt;Hi George,&lt;/P&gt;
&lt;P&gt;thank you for the feedback. Actually, from your description, it is not clear, what exactly are you proposing.&lt;/P&gt;
&lt;P&gt;The usage of the workspace or write script on different machine is described in user guide, chapter 5.1.4.2. Basically you must define your custom environment variable to use the script on different machine. This is also what SEC tool v7 does in manufacturing workspace.&lt;/P&gt;
&lt;P&gt;Hope this helps&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 07:08:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1759629#M308</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2023-11-20T07:08:22Z</dc:date>
    </item>
    <item>
      <title>Re: SEC Tool v7 write image script points to improper installation bin for different scripts.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1760018#M309</link>
      <description>&lt;P&gt;Hi Marek,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;I read the user chapter that you described. Perhaps the issue then is when we generated a manufacturing package in Linux, and used the manufacturing package on Windows, it was unable to change ${&lt;SPAN&gt;SPT_INSTALL_BIN&lt;/SPAN&gt;} to route the installation directory to the right location on the windows machine. When running the manufacturing tool in Windows, it would complain that it could not find directory '&lt;SPAN&gt;/opt/nxp/MCUX_Provi_v7/bin'&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 19:01:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1760018#M309</guid>
      <dc:creator>george_iyo</dc:creator>
      <dc:date>2023-11-20T19:01:02Z</dc:date>
    </item>
    <item>
      <title>Re: SEC Tool v7 write image script points to improper installation bin for different scripts.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1760730#M310</link>
      <description>&lt;P&gt;Hi George,&lt;/P&gt;
&lt;P&gt;I double check your use case and I confirm the bug. It is expected the tool will define SEC_INSTALL_BIN environment variable in manufacturing mode but it does not define it in version 7 nor in version 6. We will fix this for next version.&lt;/P&gt;
&lt;P&gt;Sorry for inconvenience. As a workaround, you must update the environment variable in the write script manually.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 12:07:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SEC-Tool-v7-write-image-script-points-to-improper-installation/m-p/1760730#M310</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2023-11-21T12:07:08Z</dc:date>
    </item>
  </channel>
</rss>