<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using UART for downloading the image on RT1060 board in MCUXpresso Secure Provisioning Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Using-UART-for-downloading-the-image-on-RT1060-board/m-p/1056754#M19</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use the UART via the mbed serial port on the RT1060EVK (in my case COM21) for downloading a firmware image to external XiP Flash.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/111957i24C77DC19BCE459E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I'm in serial boot mode by setting of SW7 to 0-0-0-1&lt;/P&gt;&lt;P&gt;The image is an unsigned one from SDK 2.7.1 "iled blinky".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When trying to write the image to external Flash via UART then the following error message occurs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;### Check presence of flashloader ###&lt;BR /&gt;blhost -p COM21,115200 -j -- get-property 1 0&lt;BR /&gt;{&lt;BR /&gt; "command" : "ping",&lt;BR /&gt; "response" : [],&lt;BR /&gt; "status" : {&lt;BR /&gt; "description" : "10500 (0x2904) No response received for ping command.",&lt;BR /&gt; "value" : 10500&lt;BR /&gt; }&lt;BR /&gt;}&lt;BR /&gt;blhost failed&lt;BR /&gt;Flashloader is not running yet, download and run it&lt;BR /&gt;### Check communication with target bootloader ###&lt;BR /&gt;sdphost -p COM21,115200 -j -- error-status&lt;BR /&gt;{&lt;BR /&gt; "command" : "error-status",&lt;BR /&gt; "response" : [],&lt;BR /&gt; "status" : {&lt;BR /&gt; "description" : "10004 (0x2714) No response from device.",&lt;BR /&gt; "value" : 10004&lt;BR /&gt; }&lt;BR /&gt;}&lt;BR /&gt;sdphost failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that mean for serial download via UART the Flashloader has to be run additionally as the Boot ROM in RT1060 is not sufficient?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(P.S. Download via USB works well)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;br&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jun 2020 09:08:18 GMT</pubDate>
    <dc:creator>guenter_loettrich</dc:creator>
    <dc:date>2020-06-04T09:08:18Z</dc:date>
    <item>
      <title>Using UART for downloading the image on RT1060 board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Using-UART-for-downloading-the-image-on-RT1060-board/m-p/1056754#M19</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use the UART via the mbed serial port on the RT1060EVK (in my case COM21) for downloading a firmware image to external XiP Flash.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/111957i24C77DC19BCE459E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I'm in serial boot mode by setting of SW7 to 0-0-0-1&lt;/P&gt;&lt;P&gt;The image is an unsigned one from SDK 2.7.1 "iled blinky".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When trying to write the image to external Flash via UART then the following error message occurs:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;### Check presence of flashloader ###&lt;BR /&gt;blhost -p COM21,115200 -j -- get-property 1 0&lt;BR /&gt;{&lt;BR /&gt; "command" : "ping",&lt;BR /&gt; "response" : [],&lt;BR /&gt; "status" : {&lt;BR /&gt; "description" : "10500 (0x2904) No response received for ping command.",&lt;BR /&gt; "value" : 10500&lt;BR /&gt; }&lt;BR /&gt;}&lt;BR /&gt;blhost failed&lt;BR /&gt;Flashloader is not running yet, download and run it&lt;BR /&gt;### Check communication with target bootloader ###&lt;BR /&gt;sdphost -p COM21,115200 -j -- error-status&lt;BR /&gt;{&lt;BR /&gt; "command" : "error-status",&lt;BR /&gt; "response" : [],&lt;BR /&gt; "status" : {&lt;BR /&gt; "description" : "10004 (0x2714) No response from device.",&lt;BR /&gt; "value" : 10004&lt;BR /&gt; }&lt;BR /&gt;}&lt;BR /&gt;sdphost failed&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that mean for serial download via UART the Flashloader has to be run additionally as the Boot ROM in RT1060 is not sufficient?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(P.S. Download via USB works well)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;br&lt;/P&gt;&lt;P&gt;Guenter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 09:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Using-UART-for-downloading-the-image-on-RT1060-board/m-p/1056754#M19</guid>
      <dc:creator>guenter_loettrich</dc:creator>
      <dc:date>2020-06-04T09:08:18Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART for downloading the image on RT1060 board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Using-UART-for-downloading-the-image-on-RT1060-board/m-p/1056755#M20</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guenter,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there should not be any major difference for UART, it should work same way as USB. Flashloader should be downloaded automatically by the write script.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please double check, UART is correctly selected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can also try on command-line using &lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;sdphost -p COM21,115200 -j -- error-status&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;whether connection with the ROM Bootloader can be established.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 15:59:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Using-UART-for-downloading-the-image-on-RT1060-board/m-p/1056755#M20</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2020-06-04T15:59:42Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART for downloading the image on RT1060 board</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Using-UART-for-downloading-the-image-on-RT1060-board/m-p/1056756#M21</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hi Marek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;issue&lt;/SPAN&gt; &lt;SPAN&gt;is&lt;/SPAN&gt; &lt;SPAN&gt;solved&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="mso-ansi-language:EN-US"&gt;It is not allowed to have USB OTG and UART connection at the same time. USB then seems to get precedence over UART.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="mso-ansi-language:EN-US"&gt;Unplugging the USB cable from J9 made it work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="mso-ansi-language:EN-US"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="mso-ansi-language:EN-US"&gt;Would that be worth putting a NOTE into the documentation?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="mso-ansi-language:EN-US"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN lang="EN-US" style="mso-ansi-language:EN-US"&gt;br&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="mso-ansi-language:EN-US"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="mso-ansi-language:EN-US"&gt;Guenter&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2020 07:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Using-UART-for-downloading-the-image-on-RT1060-board/m-p/1056756#M21</guid>
      <dc:creator>guenter_loettrich</dc:creator>
      <dc:date>2020-06-05T07:12:20Z</dc:date>
    </item>
  </channel>
</rss>