<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [SecureProvisioningTool] Can not boot binary if axf file is used for build image in MCUXpresso Secure Provisioning Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SecureProvisioningTool-Can-not-boot-binary-if-axf-file-is-used/m-p/1042769#M18</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I solved the issue after reinstall the Secure provisioning Tool now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hiroshi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Jul 2020 01:34:19 GMT</pubDate>
    <dc:creator>hiroshihiraga</dc:creator>
    <dc:date>2020-07-17T01:34:19Z</dc:date>
    <item>
      <title>[SecureProvisioningTool] Can not boot binary if axf file is used for build image</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SecureProvisioningTool-Can-not-boot-binary-if-axf-file-is-used/m-p/1042768#M17</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i tried to build the image of axf file with unsigned boot type, it won't boot the binary from Flash correctly.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did build the image on MCUXPresso IDE with the preprocessor define, XIP_BOOT_HEADER_ENABLE =0, and debug console is set to UART instead of semihosting.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115729i4C4922153DA10539/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then, go back to the Secure provisioning tool, "Boot Type" is selected to "unsigned" and Boot Device is selected to "Flex-spi-nor/IS25LPxxxA_IS25WPxxxA".&lt;/P&gt;&lt;P&gt;Then, select the binary, MIMXRT1062xxxxA_Project_XIP.axf. I can find the start address which is 0x60002000 and it should be correct.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115730iA626DE5CEA544BA9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then, finally I program the unsigned binary image in the flash using the "Write Image" tab.&lt;/P&gt;&lt;P&gt;It was done successfully without any fail.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115731iD38CA862005935F5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, it doesn't boot the binary correctly, meaning it won't show "Hello World" in the terminal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I select .bin file instead of .axf file when I build the image on the SecurepProvisioningTool and specify the correct start address by manual, It boots up correctly in the same manner of writing the image in Flash above.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why axf file can not be used for my case?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hiroshi,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2020 07:06:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SecureProvisioningTool-Can-not-boot-binary-if-axf-file-is-used/m-p/1042768#M17</guid>
      <dc:creator>hiroshihiraga</dc:creator>
      <dc:date>2020-07-14T07:06:24Z</dc:date>
    </item>
    <item>
      <title>Re: [SecureProvisioningTool] Can not boot binary if axf file is used for build image</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SecureProvisioningTool-Can-not-boot-binary-if-axf-file-is-used/m-p/1042769#M18</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I solved the issue after reinstall the Secure provisioning Tool now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Hiroshi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2020 01:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/SecureProvisioningTool-Can-not-boot-binary-if-axf-file-is-used/m-p/1042769#M18</guid>
      <dc:creator>hiroshihiraga</dc:creator>
      <dc:date>2020-07-17T01:34:19Z</dc:date>
    </item>
  </channel>
</rss>