<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Secure Provisioning Tool V5 b220825 in MCUXpresso Secure Provisioning Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provisioning-Tool-V5-b220825/m-p/1526727#M160</link>
    <description>&lt;P&gt;Hello, good to hear the problem is resolved. Unfortunately we cannot rebuild the Provisioning Tool, because on the particular MSVC depends 3rd party SW used in the product and not the Secure Provisioning tool itself.&lt;/P&gt;
&lt;P&gt;Also one can try to install manually the MSCV from &lt;A class="external-link" href="https://www.microsoft.com/en-us/download/details.aspx?id=48145" rel="nofollow" data-fm-marker="78" target="_blank"&gt;https://www.microsoft.com/en-us/download/details.aspx?id=48145&lt;/A&gt; and resolve potential conflicts in advance before the Secure Prov. tool is installed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
    <pubDate>Thu, 22 Sep 2022 11:20:12 GMT</pubDate>
    <dc:creator>liborukropec</dc:creator>
    <dc:date>2022-09-22T11:20:12Z</dc:date>
    <item>
      <title>Secure Provisioning Tool V5 b220825</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provisioning-Tool-V5-b220825/m-p/1526146#M159</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am unable to install Secure Provisioning Tool v5 because it depends on VC2015 v14.0.23026 but my system already has VC2015-2019 v14.28.29913&lt;/P&gt;&lt;P&gt;Can anyone at NXP rebuild the Provisioning Tool v5 to work with VC2015 v14.0 or higher?&lt;/P&gt;&lt;P&gt;I cannot uninstall v14.28 because other programs are using it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;This is crazy but solved my problem. I installed Provisioning Tool v4.1.1 and then I tried to install v5 and this time it worked! Looks like that as an upgrade from v4.1.1 to v5 it did not care about the VC2015 version.&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Sep 2022 20:09:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provisioning-Tool-V5-b220825/m-p/1526146#M159</guid>
      <dc:creator>gilmotta2</dc:creator>
      <dc:date>2022-09-21T20:09:54Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Provisioning Tool V5 b220825</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provisioning-Tool-V5-b220825/m-p/1526727#M160</link>
      <description>&lt;P&gt;Hello, good to hear the problem is resolved. Unfortunately we cannot rebuild the Provisioning Tool, because on the particular MSVC depends 3rd party SW used in the product and not the Secure Provisioning tool itself.&lt;/P&gt;
&lt;P&gt;Also one can try to install manually the MSCV from &lt;A class="external-link" href="https://www.microsoft.com/en-us/download/details.aspx?id=48145" rel="nofollow" data-fm-marker="78" target="_blank"&gt;https://www.microsoft.com/en-us/download/details.aspx?id=48145&lt;/A&gt; and resolve potential conflicts in advance before the Secure Prov. tool is installed.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
      <pubDate>Thu, 22 Sep 2022 11:20:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-Provisioning-Tool-V5-b220825/m-p/1526727#M160</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2022-09-22T11:20:12Z</dc:date>
    </item>
  </channel>
</rss>