<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MBDT for VISION中的主题 NXP  S3V234 SBC : Sony Camera IMX224 run opencv application, no /dev/video file</title>
    <link>https://community.nxp.com/t5/MBDT-for-VISION/NXP-S3V234-SBC-Sony-Camera-IMX224-run-opencv-application-no-dev/m-p/1232447#M287</link>
    <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;I am using the NXP S32V234 SBC with an attached Sony IMX224 Image sensor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;In order to use any opencv program I need to see the camera device mapped onto /dev. I can only find /dev/cam_generic on my system. There is no /dev/video* on my system.&lt;/P&gt;&lt;P&gt;How can I run a simple video capture opencv example, because the standard interfaces are not supported here.&lt;/P&gt;&lt;P&gt;All the necessary drivers are installed from the VSDK installation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do I need to update my boot files to enable this or make any other configuration changes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No devices are listed when this command is executed.&lt;/P&gt;&lt;P&gt;v4l2-ctl --list-devices&lt;BR /&gt;Failed to open /dev/video0: No such file or directory&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PS: I checked the NXP demo code. They are not helpful since they use memory mapped devices and this is not helpful for running more common opencv programs.&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 18 Feb 2021 03:16:11 GMT</pubDate>
    <dc:creator>dakshina_dasari</dc:creator>
    <dc:date>2021-02-18T03:16:11Z</dc:date>
    <item>
      <title>NXP  S3V234 SBC : Sony Camera IMX224 run opencv application, no /dev/video file</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/NXP-S3V234-SBC-Sony-Camera-IMX224-run-opencv-application-no-dev/m-p/1232447#M287</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;I am using the NXP S32V234 SBC with an attached Sony IMX224 Image sensor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;In order to use any opencv program I need to see the camera device mapped onto /dev. I can only find /dev/cam_generic on my system. There is no /dev/video* on my system.&lt;/P&gt;&lt;P&gt;How can I run a simple video capture opencv example, because the standard interfaces are not supported here.&lt;/P&gt;&lt;P&gt;All the necessary drivers are installed from the VSDK installation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do I need to update my boot files to enable this or make any other configuration changes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;No devices are listed when this command is executed.&lt;/P&gt;&lt;P&gt;v4l2-ctl --list-devices&lt;BR /&gt;Failed to open /dev/video0: No such file or directory&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;PS: I checked the NXP demo code. They are not helpful since they use memory mapped devices and this is not helpful for running more common opencv programs.&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Feb 2021 03:16:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/NXP-S3V234-SBC-Sony-Camera-IMX224-run-opencv-application-no-dev/m-p/1232447#M287</guid>
      <dc:creator>dakshina_dasari</dc:creator>
      <dc:date>2021-02-18T03:16:11Z</dc:date>
    </item>
    <item>
      <title>Re: NXP  S3V234 SBC : Sony Camera IMX224 run opencv application, no /dev/video file</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/NXP-S3V234-SBC-Sony-Camera-IMX224-run-opencv-application-no-dev/m-p/1495462#M301</link>
      <description>&lt;P&gt;I've encountered the same issue and attempted several methods like cv2.VideoCapture(-1) or cv2.VideoCapture(1) but without much success.&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;I succeeded after reading&lt;SPAN&gt;&amp;nbsp;this article&lt;/SPAN&gt;&lt;SPAN&gt;:&amp;nbsp;&lt;A href="https://manivannan-ai.medium.com/live-webcam-flask-opencv-python-26a61fee831" target="_blank" rel="noopener"&gt;https://manivannan-ai.medium.com/live-webcam-flask-opencv-python-26a61fee831&lt;/A&gt;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;and&lt;SPAN&gt;&amp;nbsp;disabling debug-mode&amp;nbsp;&lt;A href="https://www.mybalancenow.biz/" target="_self"&gt;MyBalanceNow&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 27 Jul 2022 03:57:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/NXP-S3V234-SBC-Sony-Camera-IMX224-run-opencv-application-no-dev/m-p/1495462#M301</guid>
      <dc:creator>Guth55434</dc:creator>
      <dc:date>2022-07-27T03:57:38Z</dc:date>
    </item>
    <item>
      <title>Re: NXP  S3V234 SBC : Sony Camera IMX224 run opencv application, no /dev/video file</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/NXP-S3V234-SBC-Sony-Camera-IMX224-run-opencv-application-no-dev/m-p/1500341#M302</link>
      <description>&lt;P&gt;Hello&amp;nbsp;Guth55434,&lt;/P&gt;&lt;P&gt;I am also trying to start mipi csi imx224 camera in s32v234. could you please share what is the device id you used to start the camera?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Aug 2022 14:54:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/NXP-S3V234-SBC-Sony-Camera-IMX224-run-opencv-application-no-dev/m-p/1500341#M302</guid>
      <dc:creator>Jaypee</dc:creator>
      <dc:date>2022-08-03T14:54:05Z</dc:date>
    </item>
  </channel>
</rss>