<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic kernel panic when booting the s32v234sbc in MBDT for VISION</title>
    <link>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983968#M270</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, i'm not good at using English.&lt;/P&gt;&lt;P&gt;I have a s32v234sbc package and i am trying to boot it with yocto image.&lt;/P&gt;&lt;P&gt;(* VisionSDK_S32V2_RTM_1_5_0_img_yocto.tar.gz)&lt;/P&gt;&lt;P&gt;Used image is yocto origianl image(Image,&amp;nbsp;fsl-s32v234sbc.dtb, u-boot.s32)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;however, always kernel panic occurs&amp;nbsp;as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please, let me know how to figure out it.&lt;/P&gt;&lt;P&gt;* i already check that kernel panic occurs when loading the seq.ko module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;U-Boot 2018.07+g21d6118 (Sep 24 2019 - 18:09:50 +0000)&lt;/P&gt;&lt;P&gt;CPU: NXP S32V234 V2.0 at 1000 MHz&lt;BR /&gt;Reset cause: Software Functional reset&lt;BR /&gt;Board: mpxs32v234-R2&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;RTC: PCF85263&lt;BR /&gt;All (4) cores are up.&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;/P&gt;&lt;P&gt;Forcing PCIe to Gen1 operation&lt;BR /&gt;phy link never came up&lt;BR /&gt;DEBUG_R0: 0x007dc100, DEBUG_R1: 0x08200000&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;** Unable to read file cse.bin **&lt;BR /&gt;CSE firmware loading failed&lt;BR /&gt;Failed to initialize CSE3 security engine&lt;BR /&gt;Net: FEC&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;8767496 bytes read in 416 ms (20.1 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;21981 bytes read in 18 ms (1.2 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 82000000&lt;BR /&gt; Booting using the fdt blob at 0x82000000&lt;BR /&gt; reserving fdt memory region: addr=80000000 size=10000&lt;BR /&gt; Loading Device Tree to 000000009fff7000, end 000000009ffff5dc ... OK&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]&lt;BR /&gt;[ 0.000000] Linux version 4.19.31-rt18+g9efc51a (oe-user@oe-host) (gcc version 6.3.1 20170509 (Linaro GCC 6.3-2017.06~dev)) #1 SMP Tue Sep 24 18:10:27 UTC 2019&lt;BR /&gt;[ 0.000000] Machine model: Freescale S32V234&lt;BR /&gt;[ 0.000000] cma: Reserved 32 MiB at 0x00000000fe000000&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0xa4/0x400 with crng_init=0&lt;BR /&gt;[ 0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s49688 r8192 d32232 u90112&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;INIT: version 2.88 booting&lt;BR /&gt;[ 1.241503] random: fast init done&lt;BR /&gt;[ 1.430363] apex: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 1.437668] APEX kernel module - IRQ 34, ID 0, 1 devices loaded.&lt;BR /&gt;[ 1.443459] APEX kernel module - IRQ 35, ID 1, 2 devices loaded.&lt;BR /&gt;[ 1.687735] Managing the chunk [0x89000000 - 0x8fd00000]&lt;BR /&gt;[ 1.687735] (align = 0x1000, id = 0, autobalance = 1, init = 0)&lt;BR /&gt;[ 1.698852] Managing the chunk [0xc9000000 - 0xd0000000]&lt;BR /&gt;[ 1.698852] (align = 0x1000, id = 1, autobalance = 1, init = 0)&lt;BR /&gt;[ 1.714181] Managing the chunk [0x3e801000 - 0x3eb00000]&lt;BR /&gt;[ 1.714181] (align = 0x8, id = 2, autobalance = 0, init = 1)&lt;BR /&gt;[ 1.724960] Initializing '3e801000.oalsramS'&lt;BR /&gt;[ 1.774133] Managing the chunk [0x3eb00000 - 0x3ec00000]&lt;BR /&gt;[ 1.774133] (align = 0x8, id = 3, autobalance = 0, init = 1)&lt;BR /&gt;[ 1.784914] Initializing '3eb00000.oalsramM'&lt;BR /&gt;[ 1.900160] CSI: driver ready -&amp;gt; CSI0 = enabled | CSI1 = enabled.&lt;BR /&gt;[ 1.983458] Load sbc board configuration&lt;BR /&gt;[ 1.987307] CGD: ready.&lt;BR /&gt;[ 2.095025] SError Interrupt on CPU2, code 0xbf000002 -- SError&lt;BR /&gt;[ 2.095028] CPU: 2 PID: 763 Comm: insmod Tainted: G O 4.19.31-rt18+g9efc51a #1&lt;BR /&gt;[ 2.095030] Hardware name: Freescale S32V234 (DT)&lt;BR /&gt;[ 2.095031] pstate: 20000005 (nzCv daif -PAN -UAO)&lt;BR /&gt;[ 2.095033] pc : SeqRamsInit+0x5c/0x130 [seq]&lt;BR /&gt;[ 2.095034] lr : SEQ_DRV_Setup+0x30/0xb0 [seq]&lt;BR /&gt;[ 2.095035] sp : ffffff800b4ebb30&lt;BR /&gt;[ 2.095037] x29: ffffff800b4ebb30 x28: 000000000000002f&lt;BR /&gt;[ 2.095041] x27: ffffffc07aedddd0 x26: ffffff8000c30550&lt;BR /&gt;[ 2.095044] x25: ffffff8000c30188 x24: ffffff80088e0000&lt;BR /&gt;[ 2.095047] x23: ffffff8000c30500 x22: ffffff8000c30000&lt;BR /&gt;[ 2.095051] x21: ffffff8000c30000 x20: ffffff8000c30000&lt;BR /&gt;[ 2.095054] x19: ffffff8000c30808 x18: ffffffffffffffff&lt;BR /&gt;[ 2.095057] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 2.095061] x15: 0000000000000400 x14: 0000000000000400&lt;BR /&gt;[ 2.095064] x13: 0000000000000000 x12: 0000000000000001&lt;BR /&gt;[ 2.095067] x11: 0000000000026374 x10: 0000000001077b93&lt;BR /&gt;[ 2.095071] x9 : 0000000000000138 x8 : ffffffc07dfce040&lt;BR /&gt;[ 2.095074] x7 : 0000000000000000 x6 : ffffff8008895368&lt;BR /&gt;[ 2.095077] x5 : 0000000000000000 x4 : 0000000000000000&lt;BR /&gt;[ 2.095081] x3 : ffffff8008a45000 x2 : ffffff8000c30000&lt;BR /&gt;[ 2.095084] x1 : ffffff8008a66000 x0 : ffffff8008a65017&lt;BR /&gt;[ 2.095088] Kernel panic - not syncing: Asynchronous SError Interrupt&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Mar 2020 08:18:33 GMT</pubDate>
    <dc:creator>nskang</dc:creator>
    <dc:date>2020-03-18T08:18:33Z</dc:date>
    <item>
      <title>kernel panic when booting the s32v234sbc</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983968#M270</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry, i'm not good at using English.&lt;/P&gt;&lt;P&gt;I have a s32v234sbc package and i am trying to boot it with yocto image.&lt;/P&gt;&lt;P&gt;(* VisionSDK_S32V2_RTM_1_5_0_img_yocto.tar.gz)&lt;/P&gt;&lt;P&gt;Used image is yocto origianl image(Image,&amp;nbsp;fsl-s32v234sbc.dtb, u-boot.s32)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;however, always kernel panic occurs&amp;nbsp;as below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please, let me know how to figure out it.&lt;/P&gt;&lt;P&gt;* i already check that kernel panic occurs when loading the seq.ko module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;U-Boot 2018.07+g21d6118 (Sep 24 2019 - 18:09:50 +0000)&lt;/P&gt;&lt;P&gt;CPU: NXP S32V234 V2.0 at 1000 MHz&lt;BR /&gt;Reset cause: Software Functional reset&lt;BR /&gt;Board: mpxs32v234-R2&lt;BR /&gt;I2C: ready&lt;BR /&gt;DRAM: 2 GiB&lt;BR /&gt;RTC: PCF85263&lt;BR /&gt;All (4) cores are up.&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;Failed (-5)&lt;/P&gt;&lt;P&gt;Forcing PCIe to Gen1 operation&lt;BR /&gt;phy link never came up&lt;BR /&gt;DEBUG_R0: 0x007dc100, DEBUG_R1: 0x08200000&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;** Unable to read file cse.bin **&lt;BR /&gt;CSE firmware loading failed&lt;BR /&gt;Failed to initialize CSE3 security engine&lt;BR /&gt;Net: FEC&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;switch to partitions #0, OK&lt;BR /&gt;mmc0 is current device&lt;BR /&gt;8767496 bytes read in 416 ms (20.1 MiB/s)&lt;BR /&gt;Booting from mmc ...&lt;BR /&gt;21981 bytes read in 18 ms (1.2 MiB/s)&lt;BR /&gt;## Flattened Device Tree blob at 82000000&lt;BR /&gt; Booting using the fdt blob at 0x82000000&lt;BR /&gt; reserving fdt memory region: addr=80000000 size=10000&lt;BR /&gt; Loading Device Tree to 000000009fff7000, end 000000009ffff5dc ... OK&lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]&lt;BR /&gt;[ 0.000000] Linux version 4.19.31-rt18+g9efc51a (oe-user@oe-host) (gcc version 6.3.1 20170509 (Linaro GCC 6.3-2017.06~dev)) #1 SMP Tue Sep 24 18:10:27 UTC 2019&lt;BR /&gt;[ 0.000000] Machine model: Freescale S32V234&lt;BR /&gt;[ 0.000000] cma: Reserved 32 MiB at 0x00000000fe000000&lt;BR /&gt;[ 0.000000] random: get_random_bytes called from start_kernel+0xa4/0x400 with crng_init=0&lt;BR /&gt;[ 0.000000] percpu: Embedded 22 pages/cpu @(____ptrval____) s49688 r8192 d32232 u90112&lt;BR /&gt;[ 0.000000] Detected VIPT I-cache on CPU0&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;INIT: version 2.88 booting&lt;BR /&gt;[ 1.241503] random: fast init done&lt;BR /&gt;[ 1.430363] apex: loading out-of-tree module taints kernel.&lt;BR /&gt;[ 1.437668] APEX kernel module - IRQ 34, ID 0, 1 devices loaded.&lt;BR /&gt;[ 1.443459] APEX kernel module - IRQ 35, ID 1, 2 devices loaded.&lt;BR /&gt;[ 1.687735] Managing the chunk [0x89000000 - 0x8fd00000]&lt;BR /&gt;[ 1.687735] (align = 0x1000, id = 0, autobalance = 1, init = 0)&lt;BR /&gt;[ 1.698852] Managing the chunk [0xc9000000 - 0xd0000000]&lt;BR /&gt;[ 1.698852] (align = 0x1000, id = 1, autobalance = 1, init = 0)&lt;BR /&gt;[ 1.714181] Managing the chunk [0x3e801000 - 0x3eb00000]&lt;BR /&gt;[ 1.714181] (align = 0x8, id = 2, autobalance = 0, init = 1)&lt;BR /&gt;[ 1.724960] Initializing '3e801000.oalsramS'&lt;BR /&gt;[ 1.774133] Managing the chunk [0x3eb00000 - 0x3ec00000]&lt;BR /&gt;[ 1.774133] (align = 0x8, id = 3, autobalance = 0, init = 1)&lt;BR /&gt;[ 1.784914] Initializing '3eb00000.oalsramM'&lt;BR /&gt;[ 1.900160] CSI: driver ready -&amp;gt; CSI0 = enabled | CSI1 = enabled.&lt;BR /&gt;[ 1.983458] Load sbc board configuration&lt;BR /&gt;[ 1.987307] CGD: ready.&lt;BR /&gt;[ 2.095025] SError Interrupt on CPU2, code 0xbf000002 -- SError&lt;BR /&gt;[ 2.095028] CPU: 2 PID: 763 Comm: insmod Tainted: G O 4.19.31-rt18+g9efc51a #1&lt;BR /&gt;[ 2.095030] Hardware name: Freescale S32V234 (DT)&lt;BR /&gt;[ 2.095031] pstate: 20000005 (nzCv daif -PAN -UAO)&lt;BR /&gt;[ 2.095033] pc : SeqRamsInit+0x5c/0x130 [seq]&lt;BR /&gt;[ 2.095034] lr : SEQ_DRV_Setup+0x30/0xb0 [seq]&lt;BR /&gt;[ 2.095035] sp : ffffff800b4ebb30&lt;BR /&gt;[ 2.095037] x29: ffffff800b4ebb30 x28: 000000000000002f&lt;BR /&gt;[ 2.095041] x27: ffffffc07aedddd0 x26: ffffff8000c30550&lt;BR /&gt;[ 2.095044] x25: ffffff8000c30188 x24: ffffff80088e0000&lt;BR /&gt;[ 2.095047] x23: ffffff8000c30500 x22: ffffff8000c30000&lt;BR /&gt;[ 2.095051] x21: ffffff8000c30000 x20: ffffff8000c30000&lt;BR /&gt;[ 2.095054] x19: ffffff8000c30808 x18: ffffffffffffffff&lt;BR /&gt;[ 2.095057] x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;[ 2.095061] x15: 0000000000000400 x14: 0000000000000400&lt;BR /&gt;[ 2.095064] x13: 0000000000000000 x12: 0000000000000001&lt;BR /&gt;[ 2.095067] x11: 0000000000026374 x10: 0000000001077b93&lt;BR /&gt;[ 2.095071] x9 : 0000000000000138 x8 : ffffffc07dfce040&lt;BR /&gt;[ 2.095074] x7 : 0000000000000000 x6 : ffffff8008895368&lt;BR /&gt;[ 2.095077] x5 : 0000000000000000 x4 : 0000000000000000&lt;BR /&gt;[ 2.095081] x3 : ffffff8008a45000 x2 : ffffff8000c30000&lt;BR /&gt;[ 2.095084] x1 : ffffff8008a66000 x0 : ffffff8008a65017&lt;BR /&gt;[ 2.095088] Kernel panic - not syncing: Asynchronous SError Interrupt&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 08:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983968#M270</guid>
      <dc:creator>nskang</dc:creator>
      <dc:date>2020-03-18T08:18:33Z</dc:date>
    </item>
    <item>
      <title>Re: kernel panic when booting the s32v234sbc</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983969#M271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/stefans"&gt;stefans&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do you know what might be wrong here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 11:55:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983969#M271</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2020-03-18T11:55:43Z</dc:date>
    </item>
    <item>
      <title>Re: kernel panic when booting the s32v234sbc</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983970#M272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Root cause might be related to missing cse.bin. If the device is security enabled (which is true for latest SBCs) seq.ko will fail loading.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Stefan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 11:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983970#M272</guid>
      <dc:creator>stefans</dc:creator>
      <dc:date>2020-03-20T11:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: kernel panic when booting the s32v234sbc</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983971#M273</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;i got it your said's mean.&lt;/P&gt;&lt;P&gt;but, i'm not sure that what shall i do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;i&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;already said that i used yocto binary image from web.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;how can i solve this problem.?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 02:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983971#M273</guid>
      <dc:creator>nskang</dc:creator>
      <dc:date>2020-03-23T02:59:18Z</dc:date>
    </item>
    <item>
      <title>Re: kernel panic when booting the s32v234sbc</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983972#M274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="23863" data-objecttype="3" href="https://community.nxp.com/people/stefans" style="color: #3d9ce7; background-color: #ffffff; border: 0px; padding: 1px 0px 1px calc(12px + 0.35ex);"&gt;Stefan Schwarz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;many thanks for your answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm in a trouble still playing demo with SBC-S32V234 board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;i can't anything with it.&lt;/P&gt;&lt;P&gt;i hope that you assist me to solve my issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Issue 1.&lt;/P&gt;&lt;P&gt;As you know My SBC-S32V234 board can't boot with Yocto binary Image which is downloaded from NXP web.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;lt;You already answered about this issue&amp;gt;&lt;/P&gt;&lt;P&gt;but i can't make cse.bin file because i only have a u-boot.s32(&lt;SPAN style="background-color: #ffffff; color: #51626f; "&gt;Yocto)&lt;/SPAN&gt;&amp;nbsp;Image not Yocto source code.&amp;nbsp;&lt;/P&gt;&lt;P&gt;so, if you know that how to change&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;device security option from enable to disable. please let me know. i will try.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Issue 2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Always SBC-S32V234 board hangs with "Buffer overrun" message&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f;"&gt;when executing a sample application(elf)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;System Infomation&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;* u-boot.s32 :&amp;nbsp;v2018.07_bsp23.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp; kernel :&amp;nbsp;v4.19.59_bsp23.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp; 10 kernel modules&amp;nbsp;(&lt;SPAN&gt;viulite, jpegdcd,cam,csi,apex,h264dcd,h264enc,fdma,oal_cma,seq) are built manually&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;*&amp;nbsp;&lt;SPAN&gt;S32DS_Vision&lt;/SPAN&gt;&lt;SPAN&gt;_Linux_v2.0_b170913.bin&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN style="background-color: #ffffff; "&gt;&amp;nbsp;* application : isp_sonyimx224_h264enc_linux.elf (S32DS Project from Sample)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;root@s32v234sbc:~# ./my_isp_sonyimx224_h264enc_linux.elf&lt;/P&gt;&lt;P&gt;**************************************************************&lt;BR /&gt;** H264 encoder demo&lt;BR /&gt;** Description:&lt;BR /&gt;** o Sony imx224 camera (on MipiCsi_0) expected as image input.&lt;BR /&gt;** o ISP generates histogram for AEC, converts pixel format from&lt;BR /&gt;** RGB to YUV420 and trigers H264 encoding.&lt;BR /&gt;** o H264Encoded stream data are located in SRAM.&lt;BR /&gt;**&lt;BR /&gt;** Usage:&lt;BR /&gt;** o 1 parameter: number of frames to be captured and encoded.&lt;BR /&gt;** o no params =&amp;gt; 200 frames will be captured and encoded.&lt;BR /&gt;**&lt;BR /&gt;**************************************************************&lt;BR /&gt;**&lt;BR /&gt;** 200 frames will be encoded.&lt;BR /&gt;**&lt;BR /&gt;**************************************************************&lt;/P&gt;&lt;P&gt;Press Ctrl+C to terminate the demo.&lt;BR /&gt;[ 77.598909] Probing I2c client @ 0x1a on I2C bus #0.&lt;BR /&gt;[ 77.603780] Generic camera I2c driver added successfully.&lt;BR /&gt;VMAX = 745, Lines = 729, OB = 2&lt;BR /&gt;Framebuffer mapped at 0x7fb4922000.&lt;BR /&gt;*** Other error message received.&lt;BR /&gt;*** Sequencer error text:&lt;BR /&gt; Buffer overrun @4508:256&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Best regards,&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;Namsu,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2020 06:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/983972#M274</guid>
      <dc:creator>nskang</dc:creator>
      <dc:date>2020-03-25T06:55:50Z</dc:date>
    </item>
    <item>
      <title>Re: kernel panic when booting the s32v234sbc</title>
      <link>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/1189667#M286</link>
      <description>&lt;P&gt;I am also facing the same problem.&lt;/P&gt;&lt;P&gt;The solution is not clear.&lt;/P&gt;&lt;P&gt;Can you please elaborate -- how can i build the cse.bin? and where do i place it?&lt;/P&gt;&lt;P&gt;Also can i disable it for building the seq.ko?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Dakshina&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Nov 2020 10:38:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-VISION/kernel-panic-when-booting-the-s32v234sbc/m-p/1189667#M286</guid>
      <dc:creator>dakshina_dasari</dc:creator>
      <dc:date>2020-11-26T10:38:06Z</dc:date>
    </item>
  </channel>
</rss>