<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Radar FFT processing in MBDT for RADAR</title>
    <link>https://community.nxp.com/t5/MBDT-for-RADAR/Radar-FFT-processing/m-p/763725#M36</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Olivier,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the example shown&amp;nbsp;&lt;A href="https://community.nxp.com/thread/468027"&gt;Accelerate the Discrete Fourier Transform with NXP SPT &lt;/A&gt;&amp;nbsp;the number of points used for Range FFT is M=512 and for Doppler FFT is N=256, which means that one frame has N=256 chirps, and each chirp has M=512 samples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to perform the FFT algorithm, the&amp;nbsp;&lt;SPAN&gt;number of points (M and N)&lt;/SPAN&gt;&amp;nbsp;must be a power of 2. In general, the larger number the better the resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Feb 2018 08:51:49 GMT</pubDate>
    <dc:creator>iulianbulancea</dc:creator>
    <dc:date>2018-02-23T08:51:49Z</dc:date>
    <item>
      <title>Radar FFT processing</title>
      <link>https://community.nxp.com/t5/MBDT-for-RADAR/Radar-FFT-processing/m-p/763724#M35</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the number of points used to perform the range_FFT the doppler_FFT and the reason why you need this number of points&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Feb 2018 10:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-RADAR/Radar-FFT-processing/m-p/763724#M35</guid>
      <dc:creator>olivierdoare</dc:creator>
      <dc:date>2018-02-21T10:27:23Z</dc:date>
    </item>
    <item>
      <title>Re: Radar FFT processing</title>
      <link>https://community.nxp.com/t5/MBDT-for-RADAR/Radar-FFT-processing/m-p/763725#M36</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Olivier,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the example shown&amp;nbsp;&lt;A href="https://community.nxp.com/thread/468027"&gt;Accelerate the Discrete Fourier Transform with NXP SPT &lt;/A&gt;&amp;nbsp;the number of points used for Range FFT is M=512 and for Doppler FFT is N=256, which means that one frame has N=256 chirps, and each chirp has M=512 samples.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to perform the FFT algorithm, the&amp;nbsp;&lt;SPAN&gt;number of points (M and N)&lt;/SPAN&gt;&amp;nbsp;must be a power of 2. In general, the larger number the better the resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Iulian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Feb 2018 08:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-RADAR/Radar-FFT-processing/m-p/763725#M36</guid>
      <dc:creator>iulianbulancea</dc:creator>
      <dc:date>2018-02-23T08:51:49Z</dc:date>
    </item>
  </channel>
</rss>