<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MBDT for RADARのトピックRe: NXP_RADAR_Toolbox_S32R274 board</title>
    <link>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1235407#M166</link>
    <description>&lt;P&gt;The EVB is a modular development platform which can be used either as a daughter card in conjunction with the general MPC57xx motherboard or as a standalone solution. Both variants allow you to start with the software development.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.myprepaidcenter.bid/" target="_self"&gt;myprepaidcenter&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 25 Feb 2021 05:31:03 GMT</pubDate>
    <dc:creator>Batiste</dc:creator>
    <dc:date>2021-02-25T05:31:03Z</dc:date>
    <item>
      <title>NXP_RADAR_Toolbox_S32R274 board</title>
      <link>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1170324#M156</link>
      <description>&lt;P&gt;I have&amp;nbsp;NXP_RADAR_Toolbox_S32R274 board. I am able to connect this board via Ethernet&amp;nbsp;RDK Demo Controller.exe. I checked in documents related to SPT.&lt;/P&gt;&lt;P&gt;I have not clear below the points :&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;1. What is hardware interface to connection for application ?&amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;2. How can we use or connect SPT kernel etc. ? &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;3. How can I read or write data into&amp;nbsp;S32R274 board and from which interface ?&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 11:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1170324#M156</guid>
      <dc:creator>lokesha</dc:creator>
      <dc:date>2020-10-20T11:31:04Z</dc:date>
    </item>
    <item>
      <title>Re: NXP_RADAR_Toolbox_S32R274 board</title>
      <link>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1170925#M157</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I guess you are talking about this kit:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/design/designs/s32r274-end-to-end-reference-design-kit:RDK-S32R274" target="_blank"&gt;https://www.nxp.com/design/designs/s32r274-end-to-end-reference-design-kit:RDK-S32R274&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#993300"&gt;&lt;EM&gt;1. What is hardware interface to connection for application ?&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;It is Ethernet cable.&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#993300"&gt;&lt;EM&gt;2. How can we use or connect SPT kernel etc. ?&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;via Matlab&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#993300"&gt;&lt;EM&gt;3. How can I read or write data into S32R274 board and from which interface ?&lt;/EM&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;Did you go through &lt;A id="1597906755102712617505" class="" href="https://www.nxp.com/docs/en/application-note/AN12938.pdf" target="_blank" rel="noopener noreferrer"&gt;Using RSDK1.4.0 Demo Application with RDK-S32R274 or DCC Kit – Application note&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12938.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12938.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 10:07:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1170925#M157</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2020-10-21T10:07:30Z</dc:date>
    </item>
    <item>
      <title>Re: NXP_RADAR_Toolbox_S32R274 board</title>
      <link>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1172374#M158</link>
      <description>&lt;P&gt;thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I save raw ADC sample or Peak data from RDK Demo Controller GUI ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried from &lt;U&gt;Output Stream&lt;/U&gt; and Save session. but nothing saved.&lt;/P&gt;</description>
      <pubDate>Fri, 23 Oct 2020 09:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1172374#M158</guid>
      <dc:creator>lokesha</dc:creator>
      <dc:date>2020-10-23T09:17:26Z</dc:date>
    </item>
    <item>
      <title>Re: NXP_RADAR_Toolbox_S32R274 board</title>
      <link>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1172936#M159</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;there are 2 ways:&lt;/P&gt;
&lt;P&gt;With RSDK_demo, disable radar processing from the web server interface and select output of ADC data. The visualizer will receive a RTP stream with entire frame of ADC raw data&lt;/P&gt;
&lt;P&gt;if you want to save that to PC you need to modify the visualizer to do so (instead of plotting the data just save to a file.)&lt;/P&gt;
&lt;P&gt;Other way is to use 1RF_4Antenna, which by default saves data to files and just disable radar processing from config file, enable ADC output and configure the number of frames you want to dump.&lt;/P&gt;
&lt;P&gt;best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 07:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1172936#M159</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2020-10-26T07:53:51Z</dc:date>
    </item>
    <item>
      <title>Re: NXP_RADAR_Toolbox_S32R274 board</title>
      <link>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1235407#M166</link>
      <description>&lt;P&gt;The EVB is a modular development platform which can be used either as a daughter card in conjunction with the general MPC57xx motherboard or as a standalone solution. Both variants allow you to start with the software development.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.myprepaidcenter.bid/" target="_self"&gt;myprepaidcenter&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Feb 2021 05:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1235407#M166</guid>
      <dc:creator>Batiste</dc:creator>
      <dc:date>2021-02-25T05:31:03Z</dc:date>
    </item>
    <item>
      <title>Re: NXP_RADAR_Toolbox_S32R274 board</title>
      <link>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1388063#M182</link>
      <description>&lt;P&gt;Glad you like it. We have been using this for a colossal piece of a month now and it is clearly going charmingly.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.rapidfs.biz/" target="_self"&gt;Rapidfs&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Dec 2021 10:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MBDT-for-RADAR/NXP-RADAR-Toolbox-S32R274-board/m-p/1388063#M182</guid>
      <dc:creator>Ruiz256</dc:creator>
      <dc:date>2021-12-16T10:21:50Z</dc:date>
    </item>
  </channel>
</rss>