<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Unable to suspend the project or set a breakpoint in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-suspend-the-project-or-set-a-breakpoint/m-p/2039385#M9972</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221333"&gt;@FlorinCiuca&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I hope you are well. I have encountered a problem. When I export a simple Dio(one LED to toggle) project from MBDT and imported the code into S32DS. When the project is running, I could not suspend it or set a breakpoint to debug the code. Do you know what causes this and how to solve it? Attached are the error msg when I tried to suspend or set a break point to the running project. ( saying interrupt failed, or breakpoint installation failed) Many thanks, from Xiaomei&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 06 Feb 2025 15:22:23 GMT</pubDate>
    <dc:creator>XH</dc:creator>
    <dc:date>2025-02-06T15:22:23Z</dc:date>
    <item>
      <title>Unable to suspend the project or set a breakpoint</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-suspend-the-project-or-set-a-breakpoint/m-p/2039385#M9972</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221333"&gt;@FlorinCiuca&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I hope you are well. I have encountered a problem. When I export a simple Dio(one LED to toggle) project from MBDT and imported the code into S32DS. When the project is running, I could not suspend it or set a breakpoint to debug the code. Do you know what causes this and how to solve it? Attached are the error msg when I tried to suspend or set a break point to the running project. ( saying interrupt failed, or breakpoint installation failed) Many thanks, from Xiaomei&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 06 Feb 2025 15:22:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Unable-to-suspend-the-project-or-set-a-breakpoint/m-p/2039385#M9972</guid>
      <dc:creator>XH</dc:creator>
      <dc:date>2025-02-06T15:22:23Z</dc:date>
    </item>
  </channel>
</rss>