<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to set the vale of Pdu ID of Can_Write in MBDT in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-vale-of-Pdu-ID-of-Can-Write-in-MBDT/m-p/2013501#M9853</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;One way you can look at this is to consider that the &lt;EM&gt;CanHardwareObject&lt;/EM&gt; is a description of the actual hardware message buffers used for transmission.&lt;BR /&gt;&lt;EM&gt;Pdu ID&lt;/EM&gt;, NOT to be confused with &lt;EM&gt;CanObject ID&lt;/EM&gt;, is the ID of the &lt;EM&gt;CanHardwareObject&lt;/EM&gt; instance, which is the same thing as the above mentioned message buffer.&lt;BR /&gt;&lt;BR /&gt;Example:&lt;BR /&gt;If &lt;EM&gt;Pdu ID&lt;/EM&gt; is set to value 2, then &lt;EM&gt;Can_Write&lt;/EM&gt; will use the third message buffer available for transmission. &lt;BR /&gt;&lt;BR /&gt;Important: &lt;BR /&gt;In order to have more than one available message buffers, &lt;EM&gt;Can Hw Object Count&lt;/EM&gt; needs to be increased to the desired value in the Configuration Project:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Adrian_Gherca_0-1734081475255.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315788iE88A91A7BCE5AFC2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Adrian_Gherca_0-1734081475255.png" alt="Adrian_Gherca_0-1734081475255.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 13 Dec 2024 09:20:32 GMT</pubDate>
    <dc:creator>Adrian_Gherca</dc:creator>
    <dc:date>2024-12-13T09:20:32Z</dc:date>
    <item>
      <title>How to set the vale of Pdu ID of Can_Write in MBDT</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-vale-of-Pdu-ID-of-Can-Write-in-MBDT/m-p/2012756#M9850</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i was looking for an explanation on what 'Pdu ID' input value of the Can_Wrate block to give in MBDT.&lt;/P&gt;&lt;P&gt;Could anyone explain me what's this parameter and what's its purpose in the can commnication?&lt;/P&gt;&lt;P&gt;i'm using the S32K358 EVB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Simon&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Dec 2024 09:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-vale-of-Pdu-ID-of-Can-Write-in-MBDT/m-p/2012756#M9850</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2024-12-12T09:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: How to set the vale of Pdu ID of Can_Write in MBDT</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-vale-of-Pdu-ID-of-Can-Write-in-MBDT/m-p/2013501#M9853</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;One way you can look at this is to consider that the &lt;EM&gt;CanHardwareObject&lt;/EM&gt; is a description of the actual hardware message buffers used for transmission.&lt;BR /&gt;&lt;EM&gt;Pdu ID&lt;/EM&gt;, NOT to be confused with &lt;EM&gt;CanObject ID&lt;/EM&gt;, is the ID of the &lt;EM&gt;CanHardwareObject&lt;/EM&gt; instance, which is the same thing as the above mentioned message buffer.&lt;BR /&gt;&lt;BR /&gt;Example:&lt;BR /&gt;If &lt;EM&gt;Pdu ID&lt;/EM&gt; is set to value 2, then &lt;EM&gt;Can_Write&lt;/EM&gt; will use the third message buffer available for transmission. &lt;BR /&gt;&lt;BR /&gt;Important: &lt;BR /&gt;In order to have more than one available message buffers, &lt;EM&gt;Can Hw Object Count&lt;/EM&gt; needs to be increased to the desired value in the Configuration Project:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Adrian_Gherca_0-1734081475255.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/315788iE88A91A7BCE5AFC2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Adrian_Gherca_0-1734081475255.png" alt="Adrian_Gherca_0-1734081475255.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Dec 2024 09:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/How-to-set-the-vale-of-Pdu-ID-of-Can-Write-in-MBDT/m-p/2013501#M9853</guid>
      <dc:creator>Adrian_Gherca</dc:creator>
      <dc:date>2024-12-13T09:20:32Z</dc:date>
    </item>
  </channel>
</rss>