<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 MC33771C PCB does not initialize through MBDT projects. Does through GUI</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771C-PCB-does-not-initialize-through-MBDT-projects-Does/m-p/2001161#M9797</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a custom MC33771C PCB that is 14S but I have it setup to read 11S througb the connector by connecting cell 4 to 5, 6 and 7 as well. I have use a few different custom MC33771C's previously and not had any issues. However, this board is acting very weird. Whenever I try and load MBDT code onto it the device switched off straight away (Shown by VCOM light) and reports a Status of "3" from BCC_INIT. I am trying to use a single CMU with TPL.&lt;BR /&gt;&lt;BR /&gt;What is weird is that the MC33771C GUI when connected to the S32K144EVB through the MC33664 breakout board to my custom MC33771C works absolutely fine. I am just confused about what could be causing the MBDT examples from not working compared to the GUI?&lt;BR /&gt;&lt;BR /&gt;The only other this I noticed was that the voltage values seem to take a second or so to get up to the correct voltage measurement values(Video attached), is this normal?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Mon, 25 Nov 2024 13:35:51 GMT</pubDate>
    <dc:creator>Poley</dc:creator>
    <dc:date>2024-11-25T13:35:51Z</dc:date>
    <item>
      <title>MC33771C PCB does not initialize through MBDT projects. Does through GUI</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771C-PCB-does-not-initialize-through-MBDT-projects-Does/m-p/2001161#M9797</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a custom MC33771C PCB that is 14S but I have it setup to read 11S througb the connector by connecting cell 4 to 5, 6 and 7 as well. I have use a few different custom MC33771C's previously and not had any issues. However, this board is acting very weird. Whenever I try and load MBDT code onto it the device switched off straight away (Shown by VCOM light) and reports a Status of "3" from BCC_INIT. I am trying to use a single CMU with TPL.&lt;BR /&gt;&lt;BR /&gt;What is weird is that the MC33771C GUI when connected to the S32K144EVB through the MC33664 breakout board to my custom MC33771C works absolutely fine. I am just confused about what could be causing the MBDT examples from not working compared to the GUI?&lt;BR /&gt;&lt;BR /&gt;The only other this I noticed was that the voltage values seem to take a second or so to get up to the correct voltage measurement values(Video attached), is this normal?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Mon, 25 Nov 2024 13:35:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MC33771C-PCB-does-not-initialize-through-MBDT-projects-Does/m-p/2001161#M9797</guid>
      <dc:creator>Poley</dc:creator>
      <dc:date>2024-11-25T13:35:51Z</dc:date>
    </item>
  </channel>
</rss>