<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Model-Based Design Toolbox for S32K3xx 1.5.0 Deploy Issue in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-for-S32K3xx-1-5-0-Deploy-Issue/m-p/1981554#M9708</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have updated MBDT S32k3xx toolbox from 1.4 to 1.5 . After the update, deployment to the chip still go through the downloading process, however, the chip does not response. Let me know if there is an issue with setting in the configure tool or other problem that I have not resolve, thanks!&lt;/P&gt;&lt;P&gt;I have used the shared project from the community, it works great in 1.4 but encounter issue when updated to 1.5. The file is called&amp;nbsp;Article 4 - MR-CANHUBK344_CAN.zip, which you can find in the link below.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/1758456" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/1758456&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Oct 2024 23:30:57 GMT</pubDate>
    <dc:creator>Wei_H</dc:creator>
    <dc:date>2024-10-24T23:30:57Z</dc:date>
    <item>
      <title>Model-Based Design Toolbox for S32K3xx 1.5.0 Deploy Issue</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-for-S32K3xx-1-5-0-Deploy-Issue/m-p/1981554#M9708</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have updated MBDT S32k3xx toolbox from 1.4 to 1.5 . After the update, deployment to the chip still go through the downloading process, however, the chip does not response. Let me know if there is an issue with setting in the configure tool or other problem that I have not resolve, thanks!&lt;/P&gt;&lt;P&gt;I have used the shared project from the community, it works great in 1.4 but encounter issue when updated to 1.5. The file is called&amp;nbsp;Article 4 - MR-CANHUBK344_CAN.zip, which you can find in the link below.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/1758456" target="_blank"&gt;https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Communicating-over-the-CAN-Bus/ta-p/1758456&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Oct 2024 23:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Model-Based-Design-Toolbox-for-S32K3xx-1-5-0-Deploy-Issue/m-p/1981554#M9708</guid>
      <dc:creator>Wei_H</dc:creator>
      <dc:date>2024-10-24T23:30:57Z</dc:date>
    </item>
  </channel>
</rss>