<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Build Process Error in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Process-Error/m-p/1979565#M9693</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233706"&gt;@Manikandan_Raju&lt;/a&gt;&amp;nbsp;!&lt;/P&gt;
&lt;P&gt;Thank you for your interest in using MBDT!&lt;/P&gt;
&lt;P&gt;I opened the attached project and the issue with it, as stated in the Matlab Diagnostic Viewer is that there are 2 files with the same name in it. More specifically, there are 2 files named "Adc.c" inside the project, as follows:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;One is located inside the RTD/src folder and it contains the source code for the ADC driver. It is automatically included in the project when Adc blocks are used in the model.&lt;/LI&gt;
&lt;LI&gt;The second one is located inside the "Adc_ert_rtw" folder and is generated and named based on the Simulink model inside the project. In a general case, for a Simulink model named "ModelName", a "ModelName.c" and "ModelName.h" will be generated. Since the model in this case is named "Adc", an "Adc.c" is generated, resulting in conflicts.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;A quick fix for this issue would be to rename the Simulink model to something unique and more suggestive. The project should build without errors.&lt;/P&gt;
&lt;P&gt;I hope you find this explanation helpful and, if further issues occur, please don't hesitate to contact us again!&lt;/P&gt;
&lt;P&gt;Kind regards,&lt;/P&gt;
&lt;P&gt;Florin.&lt;/P&gt;</description>
    <pubDate>Tue, 22 Oct 2024 22:24:02 GMT</pubDate>
    <dc:creator>FlorinCiuca</dc:creator>
    <dc:date>2024-10-22T22:24:02Z</dc:date>
    <item>
      <title>Build Process Error</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Process-Error/m-p/1977577#M9670</link>
      <description>&lt;P&gt;Hii,&lt;/P&gt;&lt;P&gt;I am getting following error, while try to build the ADC trial project.&amp;nbsp; I have attached the Simulink file also. Anyone's help will be highly appreciated. Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Manikandan_Raju_0-1729437281873.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/305675i7800F69F393A13A3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Manikandan_Raju_0-1729437281873.png" alt="Manikandan_Raju_0-1729437281873.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Manikandan_Raju_0-1729437281873.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 20 Oct 2024 15:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Process-Error/m-p/1977577#M9670</guid>
      <dc:creator>Manikandan_Raju</dc:creator>
      <dc:date>2024-10-20T15:13:32Z</dc:date>
    </item>
    <item>
      <title>Re: Build Process Error</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Process-Error/m-p/1979565#M9693</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/233706"&gt;@Manikandan_Raju&lt;/a&gt;&amp;nbsp;!&lt;/P&gt;
&lt;P&gt;Thank you for your interest in using MBDT!&lt;/P&gt;
&lt;P&gt;I opened the attached project and the issue with it, as stated in the Matlab Diagnostic Viewer is that there are 2 files with the same name in it. More specifically, there are 2 files named "Adc.c" inside the project, as follows:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;One is located inside the RTD/src folder and it contains the source code for the ADC driver. It is automatically included in the project when Adc blocks are used in the model.&lt;/LI&gt;
&lt;LI&gt;The second one is located inside the "Adc_ert_rtw" folder and is generated and named based on the Simulink model inside the project. In a general case, for a Simulink model named "ModelName", a "ModelName.c" and "ModelName.h" will be generated. Since the model in this case is named "Adc", an "Adc.c" is generated, resulting in conflicts.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;A quick fix for this issue would be to rename the Simulink model to something unique and more suggestive. The project should build without errors.&lt;/P&gt;
&lt;P&gt;I hope you find this explanation helpful and, if further issues occur, please don't hesitate to contact us again!&lt;/P&gt;
&lt;P&gt;Kind regards,&lt;/P&gt;
&lt;P&gt;Florin.&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 22:24:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Process-Error/m-p/1979565#M9693</guid>
      <dc:creator>FlorinCiuca</dc:creator>
      <dc:date>2024-10-22T22:24:02Z</dc:date>
    </item>
    <item>
      <title>Re: Build Process Error</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Process-Error/m-p/1980199#M9701</link>
      <description>&lt;P&gt;Hii&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221333"&gt;@FlorinCiuca&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your reply, I have modified&amp;nbsp; model as per your suggestion. Now I am getting following error,&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Manikandan_Raju_0-1729686893667.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/306422iC6C87CCDC35BCE56/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Manikandan_Raju_0-1729686893667.png" alt="Manikandan_Raju_0-1729686893667.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Manikandan_Raju_0-1729686893667.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please look in to it , help me. Simulink model also attached with this.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With Regards,&lt;/P&gt;&lt;P&gt;Manikandan R.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Oct 2024 12:33:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Build-Process-Error/m-p/1980199#M9701</guid>
      <dc:creator>Manikandan_Raju</dc:creator>
      <dc:date>2024-10-23T12:33:32Z</dc:date>
    </item>
  </channel>
</rss>