<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックMIMXRT1170-EVK CAN communication not working</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVK-CAN-communication-not-working/m-p/1978970#M9685</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Long story short: I am suing the board mentioned above and the MBDT V1.3 to test the CAN communication. I am running the example "FCAN interrupts" but I don't get any response in my PCAN reading device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Long story: after I tried and failed to make this work with an "EVKB" board (see [1] below), I decided to purchase an EVK board (because the toolbox was designed for it). Once again, the simple I/O examples from the MBDT worked immediately.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to run the FCAN&amp;nbsp; interrupts example, it does compile and flash properly.&amp;nbsp; I get no response on the PCAN device connected to the board. I also disabled the "loop back self test mode" but I get no different behavior. The Flexmaster module did not work either. It shows the same error as in [1].&lt;/P&gt;&lt;P&gt;Is there some hardware modification I need to do on the board (apart from soldering the PINs?). A jumper or so, to make the CAN communication work?&lt;/P&gt;&lt;P&gt;Is there any other configuration I need to be aware of to make this work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Matlab 2019a. SDK 2.15.1., Windows 10.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any hints&lt;/P&gt;&lt;P&gt;[1] &lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVKB-CAN-and-FreeMaster-examples-not-working/m-p/1978936#M9684" target="_blank"&gt;Re: MIMXRT1170-EVKB CAN and FreeMaster examples not working - NXP Community&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 22 Oct 2024 08:11:26 GMT</pubDate>
    <dc:creator>Robinson2715</dc:creator>
    <dc:date>2024-10-22T08:11:26Z</dc:date>
    <item>
      <title>MIMXRT1170-EVK CAN communication not working</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVK-CAN-communication-not-working/m-p/1978970#M9685</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Long story short: I am suing the board mentioned above and the MBDT V1.3 to test the CAN communication. I am running the example "FCAN interrupts" but I don't get any response in my PCAN reading device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Long story: after I tried and failed to make this work with an "EVKB" board (see [1] below), I decided to purchase an EVK board (because the toolbox was designed for it). Once again, the simple I/O examples from the MBDT worked immediately.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to run the FCAN&amp;nbsp; interrupts example, it does compile and flash properly.&amp;nbsp; I get no response on the PCAN device connected to the board. I also disabled the "loop back self test mode" but I get no different behavior. The Flexmaster module did not work either. It shows the same error as in [1].&lt;/P&gt;&lt;P&gt;Is there some hardware modification I need to do on the board (apart from soldering the PINs?). A jumper or so, to make the CAN communication work?&lt;/P&gt;&lt;P&gt;Is there any other configuration I need to be aware of to make this work?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using Matlab 2019a. SDK 2.15.1., Windows 10.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for any hints&lt;/P&gt;&lt;P&gt;[1] &lt;A href="https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVKB-CAN-and-FreeMaster-examples-not-working/m-p/1978936#M9684" target="_blank"&gt;Re: MIMXRT1170-EVKB CAN and FreeMaster examples not working - NXP Community&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Oct 2024 08:11:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVK-CAN-communication-not-working/m-p/1978970#M9685</guid>
      <dc:creator>Robinson2715</dc:creator>
      <dc:date>2024-10-22T08:11:26Z</dc:date>
    </item>
  </channel>
</rss>