<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32M276SFFRD- CAN Communication in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32M276SFFRD-CAN-Communication/m-p/1978533#M9679</link>
    <description />
    <pubDate>Mon, 21 Oct 2024 21:06:52 GMT</pubDate>
    <dc:creator>Bravin_Link</dc:creator>
    <dc:date>2024-10-21T21:06:52Z</dc:date>
    <item>
      <title>S32M276SFFRD- CAN Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32M276SFFRD-CAN-Communication/m-p/1978532#M9678</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have received a S32M276SFFRD evaluation board and need to get CAN working on it. See the attached .zip file for the board details. I am following the approach of using the&amp;nbsp;s32m27x_can_receive_s32ct example that is included within NXP_MBDToolbox_S32M2xx.&amp;nbsp; This example can be found under this path:&amp;nbsp;C:\Users\username\AppData\Roaming\MathWorks\MATLAB Add-Ons\Toolboxes\NXP_MBDToolbox_S32M2xx\S32M2_Examples\can and includes a Simulink file that relies on the S32 Configuration Tool to configure the board settings. I have already been successful with interacting with the boards built in RGB LED but am struggling with getting CAN to either be transmitted or received. I have a VN5620 Vector case that I am using to hook up to the CAN H and CAN L header pins on the board to either send or receive messages on the bus. If I understand correctly there is a CAN PHY built into the microchip already, so I don't need to configure pins such as PTB0 and PTB1 as CAN rx and CAN tx. I would expect the example project to work on the evaluation board without any issue but have had no luck so far.&lt;/P&gt;&lt;P&gt;I have made sure that there is 120 ohm resistance on each end of the bus. I have verified that the baud rates on both the board and the VN5620 CAN case are the same. I have probed out the pins from the microchip to the headers to the pins on the Vector CAN case to prove there is continuity through the CAN H and CAN L lines.&lt;/P&gt;&lt;P&gt;Can you help me out with this issue? Please let me know of any additional information that is needed.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Oct 2024 21:05:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32M276SFFRD-CAN-Communication/m-p/1978532#M9678</guid>
      <dc:creator>Bravin_Link</dc:creator>
      <dc:date>2024-10-21T21:05:42Z</dc:date>
    </item>
    <item>
      <title>Re: S32M276SFFRD- CAN Communication</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32M276SFFRD-CAN-Communication/m-p/1978533#M9679</link>
      <description />
      <pubDate>Mon, 21 Oct 2024 21:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/S32M276SFFRD-CAN-Communication/m-p/1978533#M9679</guid>
      <dc:creator>Bravin_Link</dc:creator>
      <dc:date>2024-10-21T21:06:52Z</dc:date>
    </item>
  </channel>
</rss>