<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 Freemaster connection</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-connection/m-p/1971183#M9643</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;I have two models, also using URAT0 to communicate with Free Master, BMS-CAN can communicate, the other(UART) can not detect the port after burning.What caused it?!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Another problem is whether CAN1 of MPC5744P REV E is not configured with 120Ω terminal resistor. After configuring terminal resistor, I also fail to communicate with Free Master only using CAN1 channel. Is there anything I haven't configured? I use Simulink for development.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Oct 2024 08:37:53 GMT</pubDate>
    <dc:creator>Renjie-Wang</dc:creator>
    <dc:date>2024-10-10T08:37:53Z</dc:date>
    <item>
      <title>Freemaster connection</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-connection/m-p/1971183#M9643</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;I have two models, also using URAT0 to communicate with Free Master, BMS-CAN can communicate, the other(UART) can not detect the port after burning.What caused it?!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Another problem is whether CAN1 of MPC5744P REV E is not configured with 120Ω terminal resistor. After configuring terminal resistor, I also fail to communicate with Free Master only using CAN1 channel. Is there anything I haven't configured? I use Simulink for development.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 08:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Freemaster-connection/m-p/1971183#M9643</guid>
      <dc:creator>Renjie-Wang</dc:creator>
      <dc:date>2024-10-10T08:37:53Z</dc:date>
    </item>
  </channel>
</rss>