<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックiMXRT: XCP on Serial &amp;quot;'ERR_MEMORY_OVERFLOW' received in response to XCP command 'ALLOC_ODT_ENTRY'&amp;quot;</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/iMXRT-XCP-on-Serial-quot-ERR-MEMORY-OVERFLOW-received-in/m-p/1970022#M9641</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;When adding more signals to the example "evkmimxrt1060_extmode" (8x Signals in total), the model builds with the error:&lt;BR /&gt;&lt;BR /&gt;"action: EXT_CONNECT&lt;BR /&gt;Connecting to the target...&lt;BR /&gt;Model status: 2&lt;BR /&gt;External mode structural checksum received from target: [0x1907bee5, 0xc2324ddc, 0x7239595, 0x5dad94d2].&lt;BR /&gt;Target integer only code: 0&lt;BR /&gt;Enabling XCP Synchronous Data Transfer...&lt;BR /&gt;External Mode Open Protocol Connect command failed&lt;BR /&gt;Caused by:&lt;BR /&gt;ERR packet with error code 'ERR_MEMORY_OVERFLOW' received in response to XCP command 'ALLOC_ODT_ENTRY'. Target memory available for allocation to internal data structures is not sufficient. Set 'ExtModeAutomaticAllocSize' to 'on' or manually increase the target memory that is available for internal data structures."&lt;BR /&gt;&lt;BR /&gt;Attached the files for simulink.&lt;BR /&gt;&lt;BR /&gt;The issue can replicated on the EVK.&lt;BR /&gt;&lt;BR /&gt;My normal model has over 350 signals and runs fine in Freemaster, but the project is planned with XCP communication.&lt;BR /&gt;&lt;BR /&gt;DTC_Ram has already been increased over the FlexRam but when building, DTC is &lt;SPAN&gt;16852 B&lt;/SPAN&gt;.&lt;BR /&gt;&lt;BR /&gt;How does NXP recommend to resolve the issue?&amp;nbsp; It appears MBDT is already automatically allocating the memory.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Oct 2024 14:01:43 GMT</pubDate>
    <dc:creator>Sam_ECU</dc:creator>
    <dc:date>2024-10-09T14:01:43Z</dc:date>
    <item>
      <title>iMXRT: XCP on Serial "'ERR_MEMORY_OVERFLOW' received in response to XCP command 'ALLOC_ODT_ENTRY'"</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/iMXRT-XCP-on-Serial-quot-ERR-MEMORY-OVERFLOW-received-in/m-p/1970022#M9641</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;When adding more signals to the example "evkmimxrt1060_extmode" (8x Signals in total), the model builds with the error:&lt;BR /&gt;&lt;BR /&gt;"action: EXT_CONNECT&lt;BR /&gt;Connecting to the target...&lt;BR /&gt;Model status: 2&lt;BR /&gt;External mode structural checksum received from target: [0x1907bee5, 0xc2324ddc, 0x7239595, 0x5dad94d2].&lt;BR /&gt;Target integer only code: 0&lt;BR /&gt;Enabling XCP Synchronous Data Transfer...&lt;BR /&gt;External Mode Open Protocol Connect command failed&lt;BR /&gt;Caused by:&lt;BR /&gt;ERR packet with error code 'ERR_MEMORY_OVERFLOW' received in response to XCP command 'ALLOC_ODT_ENTRY'. Target memory available for allocation to internal data structures is not sufficient. Set 'ExtModeAutomaticAllocSize' to 'on' or manually increase the target memory that is available for internal data structures."&lt;BR /&gt;&lt;BR /&gt;Attached the files for simulink.&lt;BR /&gt;&lt;BR /&gt;The issue can replicated on the EVK.&lt;BR /&gt;&lt;BR /&gt;My normal model has over 350 signals and runs fine in Freemaster, but the project is planned with XCP communication.&lt;BR /&gt;&lt;BR /&gt;DTC_Ram has already been increased over the FlexRam but when building, DTC is &lt;SPAN&gt;16852 B&lt;/SPAN&gt;.&lt;BR /&gt;&lt;BR /&gt;How does NXP recommend to resolve the issue?&amp;nbsp; It appears MBDT is already automatically allocating the memory.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 14:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/iMXRT-XCP-on-Serial-quot-ERR-MEMORY-OVERFLOW-received-in/m-p/1970022#M9641</guid>
      <dc:creator>Sam_ECU</dc:creator>
      <dc:date>2024-10-09T14:01:43Z</dc:date>
    </item>
  </channel>
</rss>