<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 Changing Values Inside the Blocks in MBDT Doesn't Work</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Changing-Values-Inside-the-Blocks-in-MBDT-Doesn-t-Work/m-p/1967933#M9624</link>
    <description>&lt;P&gt;Hi, i have encoutered this issue when i try to change the value inside the blocks, for exaple Dio blocks:&lt;/P&gt;&lt;P&gt;if i change the channel to flip (for example&amp;nbsp; from the default green to red) and build, after the application is flashed, the green led still blinks instead of the red one.&lt;/P&gt;&lt;P&gt;Also in Can blocks, if i change the CanController Mode in the block it doesn't change from the default value.&lt;/P&gt;&lt;P&gt;Only if i modify the model then the changes inside the blocks became effective: for example by adding a block, commenting others...&lt;/P&gt;&lt;P&gt;I don't know why this behavior, could someone tell me how to fix this?&lt;/P&gt;&lt;P&gt;I'm using the S32K358EVB-Q289.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
    <pubDate>Mon, 07 Oct 2024 14:23:09 GMT</pubDate>
    <dc:creator>simon98</dc:creator>
    <dc:date>2024-10-07T14:23:09Z</dc:date>
    <item>
      <title>Changing Values Inside the Blocks in MBDT Doesn't Work</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Changing-Values-Inside-the-Blocks-in-MBDT-Doesn-t-Work/m-p/1967933#M9624</link>
      <description>&lt;P&gt;Hi, i have encoutered this issue when i try to change the value inside the blocks, for exaple Dio blocks:&lt;/P&gt;&lt;P&gt;if i change the channel to flip (for example&amp;nbsp; from the default green to red) and build, after the application is flashed, the green led still blinks instead of the red one.&lt;/P&gt;&lt;P&gt;Also in Can blocks, if i change the CanController Mode in the block it doesn't change from the default value.&lt;/P&gt;&lt;P&gt;Only if i modify the model then the changes inside the blocks became effective: for example by adding a block, commenting others...&lt;/P&gt;&lt;P&gt;I don't know why this behavior, could someone tell me how to fix this?&lt;/P&gt;&lt;P&gt;I'm using the S32K358EVB-Q289.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Simon&lt;/P&gt;</description>
      <pubDate>Mon, 07 Oct 2024 14:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Changing-Values-Inside-the-Blocks-in-MBDT-Doesn-t-Work/m-p/1967933#M9624</guid>
      <dc:creator>simon98</dc:creator>
      <dc:date>2024-10-07T14:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: Changing Values Inside the Blocks in MBDT Doesn't Work</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Changing-Values-Inside-the-Blocks-in-MBDT-Doesn-t-Work/m-p/1982830#M9713</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240160"&gt;@simon98&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I can confirm that the behavior you are describing is indeed present in the current Model-Based Design Toolbox version. This is on our list of future improvements and we hope to be able to improve this specific process in the next versions.&lt;/P&gt;
&lt;P&gt;For now, the best course of action in your specific use case would be to delete the "modelName_ert_rtw" folder and the "modelName.slxc" file before building the model. Doing so will trigger the code generation and update the executable based on the changes you have made inside the Model-Based Design blocks.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Robert V&lt;/P&gt;</description>
      <pubDate>Mon, 28 Oct 2024 09:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Changing-Values-Inside-the-Blocks-in-MBDT-Doesn-t-Work/m-p/1982830#M9713</guid>
      <dc:creator>robertv</dc:creator>
      <dc:date>2024-10-28T09:05:13Z</dc:date>
    </item>
  </channel>
</rss>