<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Why the Inverter Board (DEVKIT-MOTORGD) doesn't draw current in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Why-the-Inverter-Board-DEVKIT-MOTORGD-doesn-t-draw-current/m-p/1966946#M9615</link>
    <description>&lt;P&gt;Hello NXP team.&lt;/P&gt;&lt;P&gt;The Inverter board (DEVKIT-MOTORGD) That I have just bought since only a month has stopped drawing a current. Before this, it works properly and drive the motor correctly but sometimes it doesn't draw current and sometimes (mostly) it does but suddenly I found that it can't draw any current from the supply. Which part must I suspect? May it be the Gate Driver or? if it is, then what are the reasons for such probable damage of it [SW or HW]?Is there a limitation on the length of the time of triggering GD3000?&amp;nbsp;&lt;STRONG&gt;It is the second time&amp;nbsp;I loses an inverter board by the same observation in short time.&lt;/STRONG&gt; The application works on only 12V and less than 5A which is less than the rated values of the board. I uses MPC5744P MCU board.&amp;nbsp; The only change is that we made the initialization of GD3000 occurs once the code is run (once the MCU board is connected to the laptop) not after pressing start. I think this change has no effect. Please help in justifying this strange behavior.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Ahmed&lt;/P&gt;</description>
    <pubDate>Fri, 04 Oct 2024 13:48:32 GMT</pubDate>
    <dc:creator>Ahmed_Abd_El-Hafez</dc:creator>
    <dc:date>2024-10-04T13:48:32Z</dc:date>
    <item>
      <title>Why the Inverter Board (DEVKIT-MOTORGD) doesn't draw current</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Why-the-Inverter-Board-DEVKIT-MOTORGD-doesn-t-draw-current/m-p/1966946#M9615</link>
      <description>&lt;P&gt;Hello NXP team.&lt;/P&gt;&lt;P&gt;The Inverter board (DEVKIT-MOTORGD) That I have just bought since only a month has stopped drawing a current. Before this, it works properly and drive the motor correctly but sometimes it doesn't draw current and sometimes (mostly) it does but suddenly I found that it can't draw any current from the supply. Which part must I suspect? May it be the Gate Driver or? if it is, then what are the reasons for such probable damage of it [SW or HW]?Is there a limitation on the length of the time of triggering GD3000?&amp;nbsp;&lt;STRONG&gt;It is the second time&amp;nbsp;I loses an inverter board by the same observation in short time.&lt;/STRONG&gt; The application works on only 12V and less than 5A which is less than the rated values of the board. I uses MPC5744P MCU board.&amp;nbsp; The only change is that we made the initialization of GD3000 occurs once the code is run (once the MCU board is connected to the laptop) not after pressing start. I think this change has no effect. Please help in justifying this strange behavior.&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Ahmed&lt;/P&gt;</description>
      <pubDate>Fri, 04 Oct 2024 13:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Why-the-Inverter-Board-DEVKIT-MOTORGD-doesn-t-draw-current/m-p/1966946#M9615</guid>
      <dc:creator>Ahmed_Abd_El-Hafez</dc:creator>
      <dc:date>2024-10-04T13:48:32Z</dc:date>
    </item>
  </channel>
</rss>