<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックRe: MBDT</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT/m-p/1954945#M9494</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240145"&gt;@paul_ephraim_13&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;First of all, try to make sure that the MATLAB path is set correctly for the Toolbox you want to use.&lt;/P&gt;
&lt;P&gt;Try not to have other older versions of the toolbox in the path so as not to alter the functionality. Moreover, you can reset MATLAB path to default values ​​using the &lt;STRONG&gt;restoredefaultpath&lt;/STRONG&gt; command.&amp;nbsp;&lt;SPAN&gt;Keep in mind that this deletes everything you currently have in the MATLAB path. After resetting the path, from the&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;&lt;STRONG&gt;toolbox_root&lt;/STRONG&gt;&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/EM&gt;&lt;SPAN&gt;directory level you must run the&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;mbd_s32k3_path.m&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;script to set the path for the installed toolbox.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;If the path is correctly set and the error persists, try to attach screenshots with the encountered error to investigate what may be the cause of your problem.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Dragos&lt;/P&gt;</description>
    <pubDate>Mon, 16 Sep 2024 07:16:00 GMT</pubDate>
    <dc:creator>dragostoma</dc:creator>
    <dc:date>2024-09-16T07:16:00Z</dc:date>
    <item>
      <title>MBDT</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT/m-p/1953823#M9488</link>
      <description>&lt;P&gt;I AM UNABLE TO CONFIGURE NXP EXAMPLE MODELS (ADC, DIO , etc..). I am getting an error like path not specified in&amp;nbsp; Simulink , please clarify?&lt;/P&gt;</description>
      <pubDate>Fri, 13 Sep 2024 01:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT/m-p/1953823#M9488</guid>
      <dc:creator>paul_ephraim_13</dc:creator>
      <dc:date>2024-09-13T01:33:20Z</dc:date>
    </item>
    <item>
      <title>Re: MBDT</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT/m-p/1954945#M9494</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/240145"&gt;@paul_ephraim_13&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;First of all, try to make sure that the MATLAB path is set correctly for the Toolbox you want to use.&lt;/P&gt;
&lt;P&gt;Try not to have other older versions of the toolbox in the path so as not to alter the functionality. Moreover, you can reset MATLAB path to default values ​​using the &lt;STRONG&gt;restoredefaultpath&lt;/STRONG&gt; command.&amp;nbsp;&lt;SPAN&gt;Keep in mind that this deletes everything you currently have in the MATLAB path. After resetting the path, from the&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;&lt;STRONG&gt;toolbox_root&lt;/STRONG&gt;&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/EM&gt;&lt;SPAN&gt;directory level you must run the&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;mbd_s32k3_path.m&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;script to set the path for the installed toolbox.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;If the path is correctly set and the error persists, try to attach screenshots with the encountered error to investigate what may be the cause of your problem.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Dragos&lt;/P&gt;</description>
      <pubDate>Mon, 16 Sep 2024 07:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MBDT/m-p/1954945#M9494</guid>
      <dc:creator>dragostoma</dc:creator>
      <dc:date>2024-09-16T07:16:00Z</dc:date>
    </item>
  </channel>
</rss>