<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)中的主题 iMXRT: &amp;quot;ExportedGlobal&amp;quot; being defined as bss, not data</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/iMXRT-quot-ExportedGlobal-quot-being-defined-as-bss-not-data/m-p/1954733#M9491</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I have calibration values that I'd like to edit offline, therefore I'd like the labels to be first saved to flash, before being transferred to RAM.&lt;BR /&gt;&lt;BR /&gt;For all of the values I define as "ExportedGlobal" with an initial value of "0", they are then being defined as bss, not data and not being stored in Flash.&lt;BR /&gt;&lt;BR /&gt;The data type doesn't matter, boolean, unit8, single.&lt;BR /&gt;&lt;BR /&gt;How can I easily ensure&amp;nbsp; these labels are defined as data, not bss?&lt;/P&gt;</description>
    <pubDate>Sun, 15 Sep 2024 08:16:21 GMT</pubDate>
    <dc:creator>Sam_ECU</dc:creator>
    <dc:date>2024-09-15T08:16:21Z</dc:date>
    <item>
      <title>iMXRT: "ExportedGlobal" being defined as bss, not data</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/iMXRT-quot-ExportedGlobal-quot-being-defined-as-bss-not-data/m-p/1954733#M9491</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;I have calibration values that I'd like to edit offline, therefore I'd like the labels to be first saved to flash, before being transferred to RAM.&lt;BR /&gt;&lt;BR /&gt;For all of the values I define as "ExportedGlobal" with an initial value of "0", they are then being defined as bss, not data and not being stored in Flash.&lt;BR /&gt;&lt;BR /&gt;The data type doesn't matter, boolean, unit8, single.&lt;BR /&gt;&lt;BR /&gt;How can I easily ensure&amp;nbsp; these labels are defined as data, not bss?&lt;/P&gt;</description>
      <pubDate>Sun, 15 Sep 2024 08:16:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/iMXRT-quot-ExportedGlobal-quot-being-defined-as-bss-not-data/m-p/1954733#M9491</guid>
      <dc:creator>Sam_ECU</dc:creator>
      <dc:date>2024-09-15T08:16:21Z</dc:date>
    </item>
  </channel>
</rss>