<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Model-Based Design Toolbox (MBDT)のトピックSimulink missing .mot file when build for PIL</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Simulink-missing-mot-file-when-build-for-PIL/m-p/1916402#M9327</link>
    <description>&lt;P&gt;I'm using an example project to evaluate an issue I've been having when testing Processor-in-the-Loop for the &lt;LI-PRODUCT title="MPC574xB-C-G" id="MPC574xB-C-G"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;dev board. I'm able to generate the code and have it flash the board without issues with the Embedded Coder from Simulink. I ran into an error when RAppID tries to flash the board with the .mot file after starting PIL. It seems like simulink is not generating the .mot file and I can't find the setting(s) I need to change to get it to work.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; Testing so far:&lt;BR /&gt;Took the example project (gpio_mpc5748g_devkit.mdl) and flashed it with the code generator.&lt;/P&gt;&lt;P&gt;Tried to run SIL and got an error about 'PortableWordSizes' being off. Turned it on and got SIL to run&lt;/P&gt;&lt;P&gt;Tried to run PIL and got an error about a missing .mot file (included screenshots)&lt;/P&gt;</description>
    <pubDate>Wed, 24 Jul 2024 17:50:07 GMT</pubDate>
    <dc:creator>rectangle4519</dc:creator>
    <dc:date>2024-07-24T17:50:07Z</dc:date>
    <item>
      <title>Simulink missing .mot file when build for PIL</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Simulink-missing-mot-file-when-build-for-PIL/m-p/1916402#M9327</link>
      <description>&lt;P&gt;I'm using an example project to evaluate an issue I've been having when testing Processor-in-the-Loop for the &lt;LI-PRODUCT title="MPC574xB-C-G" id="MPC574xB-C-G"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;dev board. I'm able to generate the code and have it flash the board without issues with the Embedded Coder from Simulink. I ran into an error when RAppID tries to flash the board with the .mot file after starting PIL. It seems like simulink is not generating the .mot file and I can't find the setting(s) I need to change to get it to work.&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; Testing so far:&lt;BR /&gt;Took the example project (gpio_mpc5748g_devkit.mdl) and flashed it with the code generator.&lt;/P&gt;&lt;P&gt;Tried to run SIL and got an error about 'PortableWordSizes' being off. Turned it on and got SIL to run&lt;/P&gt;&lt;P&gt;Tried to run PIL and got an error about a missing .mot file (included screenshots)&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jul 2024 17:50:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/Simulink-missing-mot-file-when-build-for-PIL/m-p/1916402#M9327</guid>
      <dc:creator>rectangle4519</dc:creator>
      <dc:date>2024-07-24T17:50:07Z</dc:date>
    </item>
  </channel>
</rss>