<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MIMXRT1170-EVKB CAN and FreeMaster examples not working in Model-Based Design Toolbox (MBDT)</title>
    <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVKB-CAN-and-FreeMaster-examples-not-working/m-p/1913732#M9313</link>
    <description>&lt;DIV class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Dear NXP Community&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I am trying to use the MIMXRT1170-EVKB board with the MBDT developed by Simulink. I am having several issues while using the board with the provided examples of the NXP MBDT:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;The CANFD example "evkmimxrt1170_fcan_transfer" does not seem to send any information to the CAN network. When I flash the board with the example , the onboard LED never blinks which means that no CAN message is being sent out. I have connected a Vector CAN device to the board with a 120 ohm resistor in between. I have configured only the basic things: baud rate.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;In the same example I am trying to use FreeMASTER. The first time I run it, it seemed to briefly work. But from the second time onwards, I get an error in FreeMASTER "Can not detect the board information". I have tried similar examaples of FreeMASTER with the same result. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Some additional information:&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have tried some of the SDK examples provided in the MCU software and they worked. Specifically, I tried the hello world from the multi-core implementation.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have tried some of the GPIO from Simulink examples and they seem to work properly. Specifically, the "evkmimxrt1170_gpio_interrupt" . &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;When I connect the board, the virtual mass storage device is missing. Therefore, when I flash the board from Simulink, I used MCU link instead of OpenSDA. I provided as configuration file the one called "MIMXRT1170_SFDP_QSPI.cfx".&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I am using Windows 10, Matlab 2019B.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Any clue what I am doing wrong?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Jul 2024 06:59:07 GMT</pubDate>
    <dc:creator>Robinson2715</dc:creator>
    <dc:date>2024-07-22T06:59:07Z</dc:date>
    <item>
      <title>MIMXRT1170-EVKB CAN and FreeMaster examples not working</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVKB-CAN-and-FreeMaster-examples-not-working/m-p/1913732#M9313</link>
      <description>&lt;DIV class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Dear NXP Community&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I am trying to use the MIMXRT1170-EVKB board with the MBDT developed by Simulink. I am having several issues while using the board with the provided examples of the NXP MBDT:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;The CANFD example "evkmimxrt1170_fcan_transfer" does not seem to send any information to the CAN network. When I flash the board with the example , the onboard LED never blinks which means that no CAN message is being sent out. I have connected a Vector CAN device to the board with a 120 ohm resistor in between. I have configured only the basic things: baud rate.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;In the same example I am trying to use FreeMASTER. The first time I run it, it seemed to briefly work. But from the second time onwards, I get an error in FreeMASTER "Can not detect the board information". I have tried similar examaples of FreeMASTER with the same result. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Some additional information:&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have tried some of the SDK examples provided in the MCU software and they worked. Specifically, I tried the hello world from the multi-core implementation.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have tried some of the GPIO from Simulink examples and they seem to work properly. Specifically, the "evkmimxrt1170_gpio_interrupt" . &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;When I connect the board, the virtual mass storage device is missing. Therefore, when I flash the board from Simulink, I used MCU link instead of OpenSDA. I provided as configuration file the one called "MIMXRT1170_SFDP_QSPI.cfx".&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I am using Windows 10, Matlab 2019B.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Any clue what I am doing wrong?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jul 2024 06:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVKB-CAN-and-FreeMaster-examples-not-working/m-p/1913732#M9313</guid>
      <dc:creator>Robinson2715</dc:creator>
      <dc:date>2024-07-22T06:59:07Z</dc:date>
    </item>
    <item>
      <title>Re: MIMXRT1170-EVKB CAN and FreeMaster examples not working</title>
      <link>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVKB-CAN-and-FreeMaster-examples-not-working/m-p/1978936#M9684</link>
      <description>I have an update on this&lt;BR /&gt;&lt;BR /&gt;After some unsuccessful attempts to make it work on my side, I got feedback from NXP that the default configuration for this board is wrong, because it was made for the EVK version. So I needed to change the settings of the CAN block:&lt;BR /&gt;&lt;BR /&gt;- disabling the 'loop back self test mode',&lt;BR /&gt;&lt;BR /&gt;- changing the numbers in "propagation segment, phase segment 1, phase segment 2 and re-sync jump width" to 7,2,2,3 respectively.&lt;BR /&gt;&lt;BR /&gt;- remove the J102 and J103 on the EVKB.&lt;BR /&gt;&lt;BR /&gt;This indeed fixed the CAN Tx. However, to test the CAN Rx, I try to receive a message, and sending it back with a different ID, it does not work. I tried to put the RX block in a triggered subsystem, write to a memory location. Then, from in another triggered subsystem read from the memory location send over CAN the message. I only read random number on the other side. Any clue what could be wrong?&lt;BR /&gt;&lt;BR /&gt;With FlexMaster the problem remains. I open it from the example, go to communication wizzard, select "use direct connection to on-board USB port", select the COM port of the board (which I see in the screen), select the boud rate to which I configured the device and I get "No board detected on any of Specified UART communication port". Any clue on this?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Additional information:&lt;BR /&gt;&lt;BR /&gt;I am using Matlab R2019a, Windows 10.&lt;BR /&gt;&lt;BR /&gt;MBDT V1.3&lt;BR /&gt;&lt;BR /&gt;SDK EVKB V2.15.1&lt;BR /&gt;&lt;BR /&gt;On the board I can successfully run the basic I/O examples.</description>
      <pubDate>Tue, 22 Oct 2024 07:39:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Model-Based-Design-Toolbox-MBDT/MIMXRT1170-EVKB-CAN-and-FreeMaster-examples-not-working/m-p/1978936#M9684</guid>
      <dc:creator>Robinson2715</dc:creator>
      <dc:date>2024-10-22T07:39:43Z</dc:date>
    </item>
  </channel>
</rss>